SNVS625G February 2011 – March 2022 LM21215
PRODUCTION DATA
The output capacitor, COUT, filters the inductor ripple current and provides a source of charge for transient load conditions. A wide range of output capacitors can be used with the LM21215 that provide various advantages. The best performance is typically obtained using ceramic, SP, or OSCON type chemistries. Typical trade-offs are that the ceramic capacitor provides extremely low ESR to reduce the output ripple voltage and noise spikes, while the SP and OSCON capacitors provide a large bulk capacitance in a small volume for transient loading conditions.
When selecting the value for the output capacitor, the two performance characteristics to consider are the output voltage ripple and transient response. The output voltage ripple can be approximated by using Equation 6:
where
The amount of output ripple that can be tolerated is application specific, however, a general recommendation is to keep the output ripple less than 1% of the rated output voltage. Keep in mind ceramic capacitors are sometimes preferred because they have very low ESR, however, depending on package and voltage rating of the capacitor, the value of the capacitance can drop significantly with applied voltage. The output capacitor selection will also affect the output voltage droop during a load transient. The peak droop on the output voltage during a load transient is dependent on many factors, however, an approximation of the transient droop ignoring loop bandwidth can be obtained using Equation 7:
where
Examine both the tolerance and voltage coefficient of the capacitor when designing for a specific output ripple or transient droop target.