For best operational performance of the device, use good PCB layout practices, including:
- Noise can propagate into analog circuitry through the power pins of the circuit as a whole, as well as the operational amplifier. Bypass capacitors are used to reduce the coupled noise by providing low-impedance power sources local to the analog circuitry.
- Connect low-ESR, 0.1μF ceramic bypass capacitors
between each supply pin and ground, placed as close to the device as
possible. A single bypass capacitor from V+ to ground is
applicable for single-supply applications.
- Separate grounding for analog and digital
portions of circuitry is one of the simplest and most effective methods of noise
suppression. One or more layers on multilayer PCBs are typically devoted to
ground planes. A ground plane helps distribute heat and reduces EMI noise
pickup. Make sure to physically separate digital and analog grounds, and pay
attention to the flow of the ground current.
- To reduce parasitic coupling, run the input
traces as far away from the supply or output traces as possible. If not
possible to keep them separate, it is much better to cross the sensitive trace
perpendicular as opposed to in parallel with the noisy trace.
- Place the external components as close to the
device as possible. Keeping RF and RG close to the
inverting input minimizes parasitic capacitance,
as shown in Layout Examples.
- Keep the length of input traces as short as possible. Always remember that the input traces are the most sensitive part of the circuit.
- Consider a driven, low-impedance guard ring around the critical traces. A guard ring can significantly reduce leakage currents from nearby traces that are at different potentials.