SBOSAJ5 December 2024 TMP113
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The TMP113 resets the serial interface if the SCL line is held low by the controller or the SDA line is held low by the TMP113 for 30ms (typical) between a START and STOP condition. The TMP113 releases the SDA line if the SCL pin is pulled low and waits for a START condition from the controller. To avoid activating the timeout function, maintain a communication speed of at least 1kHz for the SCL operating frequency. If another device on the bus is holding the SDA pin low, the TMP113 does not reset.