SCDS460 june 2023 TMUX582F-SEP
ADVANCE INFORMATION
Refer to the PDF data sheet for device specific package drawings
Crosstalk (XTALK) is defined as the voltage at the source pin (Sx) of an off-switch input, when a signal is applied at the source pin of an on-switch input in the same channel, as shown in Figure 7-15 and Equation 2.