SLVSHJ8 February 2024 TPS61299-Q1
PRODUCTION DATA
The TPS61299-Q1 employs the input average current protection (OCP) function. If the inductor average current reaches the current limit threshold ILIM, the control loop can limit the inductor average current. In this case the output voltage decreases until the power balance between input and output is achieved. If the output drops below the input voltage, the TPS61299-Q1 enters into Down Mode. If the output drops below 1.6V, the TPS61299-Q1 enters into startup process again. In Pass-Through operation, input current limit function is not enabled.