The TPS6521505-Q1 offers various fault-detections. Per default, all of them lead to a sequenced shut-down. Some of them are maskable and the reaction to masked faults is configurable.
The device provides the following fault-detections on the supply voltage (VSYS) and internal voltage supply (VDD1P8):
- Undervoltage on VSYS, resulting in transition to OFF state or gating start-up
- Overvoltage-protection on VSYS, resulting in transition to OFF state
- Under- or Overvoltage on internal 1.8V-supply (VDD1P8), resulting in transition to OFF state or gating start-up.
None of these faults are maskable.
The TPS6521505-Q1 provides the following fault-detections on the buck- and LDO-outputs:
- Undervoltage detection (UV)
- Over Current detection (OC), triggering on positive as well as (for buck-converters) negative current-limit
- Short-to-GND detection (SCG)
- Temperature warning (WARM) and Thermal Shut Down (TSD / HOT)
- Residual Voltage (RV) and Residual Voltage - Shutdown (RV_SD)
- Timeout (TO)
SCG, OC, HOT, RV_SD and TO are not maskable. If any one of those occurs, the device powers down. Positive and negative current limit share the same mask-bit per regulator.
The reaction to UV, RV and WARM faults is
configurable. If not masked, a fault triggers a sequenced shut-down. UV, RV and WARM
are maskable individually per regulator in INT_MASK_BUCKS, INT_MASK_LDOS and
INT_MASK_WARM registers. No state-transition occurs in case of a masked fault.
Whether bits are set and if nINT is pulled low are globally configurable by
MASK_EFFECT bits in MASK_CONFIG register. Positive and negative current limit share
the same mask-bit per regulator.
- 00b = no state change, no nINT reaction, no bit set
- 01b = no state change, no nINT reaction, bit set
- 10b = no state change, nINT reaction, bit set (same as 11b)
- 11b = no state change, nINT reaction, bit set (same as 10b)
For any fault that corresponds to a shut-down
condition, the fault-bit remains asserted until a W1C (write-one-clear) operation is
performed via I2C (assuming the fault is not present any more). In case of a
shut-down fault, no renewed on-request is required. The device automatically
executes the power up sequence if the fault is no longer present as long as
EN/VSENSE is still high and no PB-press is required for a restart.
For any fault that is not a shut-down condition (for example because the fault is masked), the bit is cleared when going to the INITIALIZE state.
Thermal Warning and Shutdown
There are two thermal thresholds: Thermal-warning (WARM) and Thermal Shutdown (TSD / HOT).
- Thermal Warning, WARM-threshold:
- if the temperature exceeds TWARM_Rising threshold, the SENSOR_x_WARM-bit is set and the PMIC sequences down (unless masked).
- if the temperature fell below TWARM_Falling threshold, the device powers up again, without a new
Push-button-ON_Request. In EN or VSENSE configuration, the ON-request must still be valid to transition to ACTIVE state.
- if the temperature exceeds TWARM_Rising threshold, but SENSOR_x_WARM_MASK bit is /bits are set, the PMIC remains in ACTIVE state. Fault-reporting occurs as configured by MASK_EFFECT bits. The processor makes the decision to either sequence the power down or throttles back on the running applications to reduce the power consumption and hopefully avoiding a Thermal Shutdown situation.
- Thermal Shutdown, HOT-threshold, applicable if WARM-threshold is masked:
- if the temperature exceeds THOT_Rising
threshold, the SENSOR_x_HOT-bit is set and the PMIC powers off all rails
immediately. This power down is simultaneously and not sequenced.
- in case ALL sensors are masked for WARM-detection (all SENSOR_x_WARM_MASK bits are set), the PMIC does power back up once the temperature drops below the THOT_Falling threshold, provided a valid ON-request is present.
- in case any one of the sensors is unmasked for WARM-detection, the PMIC does power back up once the temperature drops below the TWARM_Falling threshold, without a new
Push-button-ON_Request. In EN or VSENSE configuration, the ON-request must still be valid to transition to ACTIVE state.
Residual Voltage
Residual voltage checks are performed at various occasions: before starting the INITIALIZE- to ACTIVE-transition and any time before a rail is enabled, regardless if during the sequence, by I2C-command or during the STBY- to ACTIVE-transition. RV-checks are also performed during the sequences, to detect if a rail that is supposed to be disabled is pulled up by another rail. The treatment of RV-faults depends on the situation when the fault occurs:
- INITIALIZE to ACTIVE:
- if residual voltage is detected for more than 4ms
to 5ms prior to the execution of the sequence, the respective
INT_RV_IS_SET bit in INT_SOURCE register and LDOx_RV respectively
BUCKx_RV bit in INT_RV register is set and remains set, even if the
discharge is successful at a later time and the ON-request is
executed.
- if the residual voltage is detected during the sequence, this constitutes a shutdown-fault: the device initiates the power-down-sequence at the end of the slot-duration. The device sets the respective INT_TIMEOUT_RV_SD_IS_SET bit in INT_SOURCE register, LDOx_RV_SD respectively BUCKx_RV_SD bit and bit TIMEOUT in INT_TIMEOUT_RV_SD register.
- ACTIVE to STBY:
- if active discharge is enabled and residual voltage is detected after eight times the power-down slot-duration, this constitutes a shutdown-fault: the device sequences down at the end of the slot. The device sets INT_TIMEOUT_RV_SD_IS_SET bit in INT_SOURCE register, the LDOx_RV_SD respectively BUCKx_RV_SD bit and the bit TIMEOUT in INT_TIMEOUT_RV_SD register.
- if the residual voltage is detected during the sequence, this constitutes a shutdown-fault: the device sequences down at the end of the slot-duration and sets bit INT_TIMEOUT_RV_SD_IS_SET in INT_SOURCE register and LDOx_RV_SD respectively BUCKx_RV_SD bit in INT_TIMEOUT_RV_SD register.
- STBY to ACTIVE:
- if residual voltage is detected prior to the
execution of the sequence for more than 4ms to 5ms, the device sets
INT_RV_IS_SET bit in INT_SOURCE register and LDOx_RV respectively
BUCKx_RV bit in INT_RV register. The bit remains set, even if the
discharge is successful before timeout expires and the
STBY-to-ACTIVE-sequence is executed.
- if residual voltage is detected for more than
80ms prior to the execution of the sequence, this constitutes a
shutdown-fault: the device sequences down and sets the bit
INT_TIMEOUT_RV_SD_IS_SET in INT_SOURCE register and LDOx_RV_SD
respectively BUCKx_RV_SD bit in INT_TIMEOUT_RV_SD register. In addition,
the device sets the bit TIMEOUT in INT_TIMEOUT_RV_SD register.
- if the residual voltage is detected during the sequence, this constitutes a shutdown-fault: the device sequences down at the end of the slot-duration and sets the INT_TIMEOUT_RV_SD_IS_SET bit in INT_SOURCE register and LDOx_RV_SD respectively BUCKx_RV_SD bit in INT_TIMEOUT_RV_SD register. The TIMEOUT bit is not set in this case.
- ACTIVE to INITIALIZE or STBY to INITIALIZE
- if the residual voltage is detected at the end of the power-down slot-duration of the respective rail, this gates the disabling of the subsequent rail for up to eight times the slot-duration, but then the power-sequence continues regardless of the residual voltage. No bit is set in this case.
- MASKING of RV-bits
- the reaction of the nINT-pin reaction in case of residual voltage detection is maskable for LDOx_RV respectively BUCKx_RV bits by MASK_INT_FOR_RV bit in MASK_CONFIG register.
- neither the bit nor the shutdown-fault-reaction in case of residual voltage detection is maskable for LDOx_RV_SD respectively BUCKx_RV_SD bits.
- Timeout
- Timeout occurs if residual voltage is not
discharged in time. The bit TIMEOUT in INT_TIMEOUT_RV_SD register is
set. See details above.
Note: In case active discharge on a rail is disabled, the unsuccessful discharge of that rail within the slot duration does not gate the disable of the subsequent rail.
During power-down, the device sets neither RV-bits nor RV_SD-bits for rails with disabled discharge.
CAUTION: For every detected Shut-Down
fault, irrespective if prior to the sequence due to unsuccessful discharge,
during the power-up-sequence or in ACTIVE or STBY state, the retry counter
(RETRY_COUNT in POWER_UP_STATUS_REG register) is incremented. The device
attempts two retries to power-up. If both fail, a power-cycle on VSYS is
required to reset the retry counter. Any successful power-up also resets the
retry counter.
If faults are
masked and do not cause a shut-down, the retry counter does not
increment.
To disable
the retry-counter, set bit MASK_RETRY_COUNT in INT_MASK_UV register. When
set, the device attempts to retry infinitely.
Below table gives an
overview of the fault-behavior in ACTIVE and STBY states if unmasked and whether a
fault is maskable.
CAUTION: Masking of faults poses a risk to
the device or the system, including but not limited to starting into a
pre-biased
output.
TI strongly recommends not to mask OC- and UV-detection on the same rail.
Table 6-6 Fault Handling
| Block |
Fault |
ACTIVE or STBY state
(if fault NOT masked) |
ACTIVE or STBY state
(if fault IS masked) |
| BUCK &
LDO |
Residual voltage -
shutdown-Fault - RV_SD *) |
Fault triggers a
sequenced shut-down to INITIALIZE state |
Not maskable |
| BUCK &
LDO |
Residual voltage -
RV |
Fault does not
trigger state-change |
Fault does not
trigger state-change |
| BUCK &
LDO |
Timeout - TO
*) |
Fault triggers a
sequenced shut-down to INITIALIZE state |
Fault does not
trigger state-change |
| BUCK &
LDO |
Undervoltage -
UV |
Fault triggers a
sequenced shut-down to INITIALIZE state |
Fault does not
trigger state-change |
| BUCK &
LDO |
Overcurrent -
OC |
Fault triggers a
sequenced shut-down to INITIALIZE state |
Not maskable |
| BUCK &
LDO |
Short-to-GND -
SCG |
Fault triggers a
sequenced shut-down to INITIALIZE state |
Not maskable |
| BUCK &
LDO |
Temperature warning
- WARM |
Fault triggers a
sequenced shut-down to INITIALIZE state |
Yes |
| BUCK &
LDO |
Temperature
shut-down - HOT |
Fault triggers an
immediate shut-down to INITIALIZE state (not sequenced) |
Not maskable |
| VSYS |
Undervoltage - UV |
Fault triggers an
immediate shut-down to OFF state (not sequenced) |
Not maskable |
| VSYS |
Overvoltage -
OV |
Fault triggers an
immediate shut-down to OFF state (not sequenced) |
Not maskable |
| VDD1P8 |
Undervoltage or
Overvoltage - UV or OV |
Fault triggers an
immediate shut-down to OFF state (not sequenced) |
Not maskable |
*) RV_SD and TIMEOUT faults only occur during a sequence