SLVSIH4 August 2025 TPS6521505-Q1
PRODUCTION DATA
The TPS6521505-Q1 offers a total of two linear regulators, LDO1 and LDO2.
LDO1: 400mA, 0.6V .. 3.4V
LDO1 is a general-purpose LDO intended to provide power to analog circuitry on the SOC or peripherals. The LDO has an input voltage range from 1.5V to 5.5V, and must be connected either directly to the system power or to the output of another converter. The output voltage is programmable in the range of 0.6V to 3.4V in 50mV-steps. The LDO supports up to 400mA. The LDO is configurable to operate in bypass-mode, acting as load-switches. If configured in bypass-mode, the desired output voltage still needs to be specified in LDOx_VOUT register. The LDOs also support output-voltage changes while enabled, supporting functions like SD-card-IO-supply, changing from 3.3V to 1.8V after initialization, either in LDO-mode at a supply-voltage above 3.3V or with a 3.3V supply changing between bypass-mode and LDO-mode. The LDO also supports Load-switch mode (LSW_mode): in this case, output voltages of 1.5V up to 5.5V are supported. The desired voltage does not need to be configured in the LDOx_VOUT register.
Alternatively, an I2C communication to VSEL_SD_I2C_CTRL in MFP_1_CONFIG register controls the change of the LDO1 output voltage.
In bypass- or LSW-mode, the LDO acts as a switch, where VOUT is VIN minus the drop over the FET-resistance (RBYPASS, RLSW).
Output Capacitance Requirements
The LDO1 regulator requires sufficient output-capacitance for stability. The required minimum and supported maximum capacitance depends on the configuration:LDO2: 300mA, 1.2V .. 3.3V
LDO2 is a general-purpose LDOs intended to provide power to analog circuitry on the SoC or peripherals. The LDO has an input voltage range from 2.2V to 5.5V, connected either directly to the system power or to the output of another converter. Note, the LDO needs a headroom between VSYS and the LDO-output voltage of minimum 150mV. The output voltage is programmable in the range of 1.2V to 3.3V in 50 mV-steps. The LDO supports up to 300mA. The LDO is configurable to act as a load-switch. In this case, output voltages of 2.2V up to 5.5V are supported. The desired voltage does not need to be configured in the LDOx_VOUT register.
The LDO supports a fast-ramp-mode with limited output capacitance and a slow-ramp-mode, allowing for larger total load capacitance.
Output Capacitance Requirements
The LDO2 regulator requires sufficient output-capacitance for stability. The required minimum and supported maximum capacitance depends on the configuration:LDO1 and LDO2
(A change between LDO and bypass-mode (supported by LDO1 only) is supported during operation.)
LDO Fault Handling
During a voltage transition (at power-up or triggered by toggling VSEL_SD-pin or an I2C-command), the device blanks the undervoltage detection by default and activates the undervoltage detection when the voltage transition completed.
If the device detects an undervoltage during the sequence into ACTIVE state (from INITIALIZE or STBY) and UV is not masked, the power-down-sequence starts at the end of the current slot.
If the device detects an undervoltage in ACTIVE-state or STBY-state and UV is not masked, the power-down sequence starts immediately. OC-detection is not maskable.
During a voltage transition (at power-up or triggered by toggling VSEL_SD-pin or an I2C-command), the overcurrent detection is blanked and gets activated when the voltage transition completed.
If the over-current occurs during the sequence into ACTIVE state (from INITIALIZE or STBY), the device disables the affected rail immediately and starts the power-down-sequence at the end of the current slot.
If the over-current occurs in ACTIVE-state or STBY-state, the device disables the affected rail immediately and starts the power-down sequence.
OC-detection is not maskable, but the deglitch-time is configurable. TI strongly recommends to use tDEGLITCH_OC_short. Extended over-current leads to increased aging or overshoot upon recovery.
SCG-detection is not maskable.
If a rail gets enabled, the device blanks SCG detection initially to allow the rail to ramp above the SCG-threshold.
| LDOx_ VSET [decimal] | LDOx_VSET [binary] | LDOx_ VSET [hexa- decimal] | VOUT (LDO1, LDO mode) [V] | VOUT (LDO1, bypass-mode) [V] | VOUT (LDO2, LDO mode) [V] |
|---|---|---|---|---|---|
|
0 |
000000 |
00 |
0.60 |
reserved |
1.20 |
|
1 |
000001 |
01 |
0.65 |
reserved |
1.20 |
|
2 |
000010 |
02 |
0.70 |
reserved |
1.20 |
|
3 |
000011 |
03 |
0.75 |
reserved |
1.20 |
|
4 |
000100 |
04 |
0.80 |
reserved |
1.20 |
|
5 |
000101 |
05 |
0.85 |
reserved |
1.20 |
|
6 |
000110 |
06 |
0.90 |
reserved |
1.20 |
|
7 |
000111 |
07 |
0.95 |
reserved |
1.20 |
|
8 |
001000 |
08 |
1.00 |
reserved |
1.20 |
|
9 |
001001 |
09 |
1.05 |
reserved |
1.20 |
|
10 |
001010 |
0A |
1.10 |
reserved |
1.20 |
|
11 |
001011 |
0B |
1.15 |
reserved |
1.20 |
|
12 |
001100 |
0C |
1.20 |
reserved |
1.20 |
|
13 |
001101 |
0D |
1.25 |
reserved |
1.25 |
|
14 |
001110 |
0E |
1.30 |
reserved |
1.30 |
|
15 |
001111 |
0F |
1.35 |
reserved |
1.35 |
|
16 |
010000 |
10 |
1.40 |
reserved |
1.40 |
|
17 |
010001 |
11 |
1.45 |
reserved |
1.45 |
|
18 |
010010 |
12 |
1.50 |
1.50 |
1.50 |
|
19 |
010011 |
13 |
1.55 |
1.55 |
1.55 |
|
20 |
010100 |
14 |
1.60 |
1.60 |
1.60 |
|
21 |
010101 |
15 |
1.65 |
1.65 |
1.65 |
|
22 |
010110 |
16 |
1.70 |
1.70 |
1.70 |
|
23 |
010111 |
17 |
1.75 |
1.75 |
1.75 |
|
24 |
011000 |
18 |
1.80 |
1.80 |
1.80 |
|
25 |
011001 |
19 |
1.85 |
1.85 |
1.85 |
|
26 |
011010 |
1A |
1.90 |
1.90 |
1.90 |
|
27 |
011011 |
1B |
1.95 |
1.95 |
1.95 |
|
28 |
011100 |
1C |
2.00 |
2.00 |
2.00 |
|
29 |
011101 |
1D |
2.05 |
2.05 |
2.05 |
|
30 |
011110 |
1E |
2.10 |
2.10 |
2.10 |
|
31 |
011111 |
1F |
2.15 |
2.15 |
2.15 |
|
32 |
100000 |
20 |
2.20 |
2.20 |
2.20 |
|
33 |
100001 |
21 |
2.25 |
2.25 |
2.25 |
|
34 |
100010 |
22 |
2.30 |
2.30 |
2.30 |
|
35 |
100011 |
23 |
2.35 |
2.35 |
2.35 |
|
36 |
100100 |
24 |
2.40 |
2.40 |
2.40 |
|
37 |
100101 |
25 |
2.45 |
2.45 |
2.45 |
|
38 |
100110 |
26 |
2.50 |
2.50 |
2.50 |
|
39 |
100111 |
27 |
2.55 |
2.55 |
2.55 |
|
40 |
101000 |
28 |
2.60 |
2.60 |
2.60 |
|
41 |
101001 |
29 |
2.65 |
2.65 |
2.65 |
|
42 |
101010 |
2A |
2.70 |
2.70 |
2.70 |
|
43 |
101011 |
2B |
2.75 |
2.75 |
2.75 |
|
44 |
101100 |
2C |
2.80 |
2.80 |
2.80 |
|
45 |
101101 |
2D |
2.85 |
2.85 |
2.85 |
|
46 |
101110 |
2E |
2.90 |
2.90 |
2.90 |
|
47 |
101111 |
2F |
2.95 |
2.95 |
2.95 |
|
48 |
110000 |
30 |
3.00 |
3.00 |
3.00 |
|
49 |
110001 |
31 |
3.05 |
3.05 |
3.05 |
|
50 |
110010 |
32 |
3.10 |
3.10 |
3.10 |
|
51 |
110011 |
33 |
3.15 |
3.15 |
3.15 |
|
52 |
110100 |
34 |
3.20 |
3.20 |
3.20 |
|
53 |
110101 |
35 |
3.25 |
3.25 |
3.25 |
|
54 |
110110 |
36 |
3.30 |
3.30 |
3.30 |
|
55 |
110111 |
37 |
3.35 |
3.35 |
3.30 |
|
56 |
111000 |
38 |
3.40 |
3.40 |
3.30 |
|
57 |
111001 |
39 |
3.40 |
3.40 |
3.30 |
|
58 |
111010 |
3A |
3.40 |
3.40 |
3.30 |
|
59 |
111011 |
3B |
3.40 |
3.40 |
3.30 |
|
60 |
111100 |
3C |
3.40 |
3.40 |
3.30 |
|
61 |
111101 |
3D |
3.40 |
3.40 |
3.30 |
|
62 |
111110 |
3E |
3.40 |
3.40 |
3.30 |
|
63 |
111111 |
3F |
3.40 |
3.40 |
3.30 |