SLUSD49A September 2017 – January 2019 UCC256303
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
This is the device over temperature protection. When OTP fault is tripped, if the device is switching, the switching will stop. If the device is in HV start up stage and JFET is on, the JFET will be turned off. Details of the OTP fault handling will be discussed in the Device Functional Modes section.
There are two digital state machines in the system:
The system states control state machine controls system operation states and faults. The waveform generator state machine controls the gate driver behavior.