JAJSRA2A December 2022 – September 2023 AFE11612-SEP
PRODUCTION DATA
The device contains one local and two remote temperature sensors. The temperature sensors continuously monitor the three temperature inputs, and new readings are automatically available every cycle. The on-chip integrated temperature sensor (shown in Figure 7-4) is used to measure the device temperature. Two remote diode sensor inputs are used to measure the two external temperatures. All analog signals are converted by the secondary ADC that runs in the background at a lower speed. The measurement relies on the characteristics of a semiconductor junction operation at a fixed current level. The forward voltage of the diode (VBE) depends on the current passing through the diode and the ambient temperature. The change in VBE when the diode operates at two different currents (a low current of ILOW and a high current of IHIGH) is shown in Equation 1:
where:
The remote sensing transistor can be a discrete, small-signal type transistor or a substrate transistor built within the microprocessor. This architecture is shown in Figure 7-5. An internal voltage source biases the D– pin above ground to prevent the ground noise from interfering with measurement. An external capacitor (up to 330 pF) can be placed between D+ and D– to further reduce noise interference.
The device has three temperature sensors: two remote (D1 and D2) and one on-chip (LT). If any sensor is not used, the sensor can be disabled by clearing the corresponding enable bit (bits D2EN, D1EN, and LTEN of the temperature configuration register). When disabled, the sensors are not converted. The device continuously monitors the selected temperature sensors in the background, leaving the user free to perform conversions on the other channels. When one monitor cycle finishes, a signal passes to the control logic to automatically initiate a new conversion.
The analog sensing signal is preprocessed by a low-pass filter and signal-conditioning circuitry, and then digitized by the ADC. The resulting digital signal is further processed by the digital filter and processing unit. The final result is stored in the LT-temperature-data register, the D1-temperature-data register, and the D2-temperature-data register, respectively. The format of the final result is in 2's complement, as shown in Table 7-1.
TEMPERATURE (°C) | DIGITAL CODE |
---|---|
+255.875 | 011111111111 |
+150 | 010010110000 |
+100 | 001100100000 |
+50 | 000110010000 |
+25 | 000011001000 |
+1 | 000000001000 |
0 | 000000000000 |
–1 | 111111111000 |
–25 | 111100111000 |
–50 | 111001110000 |
–100 | 110011100000 |
–150 | 101101010000 |
–256 | 100000000000 |