JAJSRA2A December 2022 – September 2023 AFE11612-SEP
PRODUCTION DATA
The VDRAIN voltage must be monitored to make sure that the PA drain supply is operating at the expected voltage. A resistor divider is required to properly scale the VDRAIN voltage, as the voltage range for the ADC is selected to be 0 V to 2.5 V or 0 V to 5 V. This can be accomplished using the integrated successive-approximation register (SAR) ADC in the AFE11612-SEP. SAR ADCs have an internal sampling capacitor which must be charged every time there is an ADC conversion. This capacitor must be charged within the sample acquisition time to make sure the ADC measures the voltage correctly. This is done using a charge-bucket filter with an external capacitor (CFILT) of approximately 1 nF. Limit the impedance of the resistor divider to 10 kΩ to allow sufficient current to charge the sampling capacitor.