JAJSSF8 December 2023 LDC5071-Q1
PRODUCTION DATA
While in the FAULT state, a number of parameters are continuously monitored.
For the following parameters, if a fault condition is detected, the device stays in FAULT state until and unless the fault condition is removed and then the device transitions to DIAGNOSTIC state:
For the following parameters, if a fault condition is detected, the device is transferred to the DISABLED state and a recovery is attempted (see DISABLED State):
For all other faults, the device attempts recovery by transitioning to DIAGNOSTIC state while the OUTx pins remain in FAULT signaling state.