The device enters NORMAL state after successful completion of the diagnostics checks in the DIAGNOSTICS state. In NORMAL state, the LDC5071-Q1 is fully functional and outputs valid signals at the OUT pins. These are the characteristics of the NORMAL state:
- The LC oscillator is enabled and both the oscillation frequency and amplitude are within the specified range.
- The Analog Front End is active and the frequencies of the input signals, amplitudes, and their phase relation are within the specified range.
- the AGC is fully functional and output signals are within the specified range in Auto AGC mode.
- The output stage is active and OUT pin signals are within the specified range.
- The NORMAL state diagnostics is active and running.
The device transitions from the NORMAL state to one of the following:
- FAULT state, if certain fault conditions are detected.
- DISABLED state, if certain fault conditions are detected.
See Diagnostics for more information.