JAJSHI3C March 2019 – October 2019 TPS23881
PRODUCTION DATA.
COMMAND = 26h with 1 Data Byte, Read/Write
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Physical Channel # of Logical Channel 4 | Physical Channel # of Logical Channel 3 | Physical Channel # of Logical Channel 2 | Physical Channel # of Logical Channel 1 | ||||
R/W-1 | R/W-1 | R/W-1 | R/W-0 | R/W-0 | R/W-1 | R/W-0 | R/W-0 |
LEGEND: R/W = Read/Write; R = Read only; W = Write only; CR = Clear on Read; -n = value after reset |
Bit | Field | Type | POR / RST | Description | |||||
---|---|---|---|---|---|---|---|---|---|
7–0 | Physical Channel # of Logical Channel n | R/W | 1110 0100b / P | Used to re-map channels logically due to physical board constraints. Re-mapping is between any channel within 4-channel group (1-4 or 5-8). All channels of a group of four must be in OFF mode prior to receiving the port re-mapping command, otherwise the command will be ignored. By default there is no re-mapping.
Each pair of bits corresponds to the logical port assigned. The selection per port is as follows: |
|||||
Re-Map Code | Physical Channel | Package Pins | |||||||
0 | 0 | 1 | Drain1,Gat1,Sen1 | ||||||
0 | 1 | 2 | Drain2,Gat2,Sen2 | ||||||
1 | 0 | 3 | Drain3,Gat3,Sen3 | ||||||
1 | 1 | 4 | Drain4,Gat4,Sen4 | ||||||
When there is no re-mapping the default value of this register is 1110,0100. The 2 MSbits with a value 11 indicate that logical channel 4 is mapped onto physical channel #4, the next 2 bits, 10, suggest logical channel 3 is mapped onto physical channel #3 and so on.
Note: Code duplication is not allowed – that is, the same code cannot be written into the remapping bits of more than one port – if such a value is received, it will be ignored and the chip will stay with existing configuration. Note: Port remapping configuration is kept unchanged if 0x1A IC reset command is received. |
SPACE
NOTE
The RST condition of "P" indicates that the previous state of these bits will be preserved following a device reset using the RESET pin. Thus, pulling the RESET input low will not overwrite any user changes to this register.
NOTE
Only logical Channels 3 and 4 and 1 and 2 may be wired as 4-pair Ports. Unpredictable behavior will occur if any other combinations of logical Channels are wired in a 4-pair configuration.
NOTE
After port remapping, TI recommends to do at least one detection-classification cycle before turn on.