JAJSJU6 September 2020 TPS65982DMC
PRODUCTION DATA
The TPS65982DMC has two I2C interface ports. I2C Port 1 is comprised of the I2C_SDA1, I2C_SCL1, and I2C_IRQ1Z pins. I2C Port 2 is comprised of the I2C_SDA2, I2C_SCL2, and I2C_IRQ2Z pins. These interfaces provide general status information about the TPS65982DMC, the ability to control the TPS65982DMC behavior, as well as providing control of system PD controllers.
The two ports can be a master or a slave, but the default behavior is to be a slave. Port 1 and Port 2 are interchangeable. Each port operates the same way and has the same access in and out of the core. An interrupt mask is set for each that determines what events are interrupted on that given port.