JAJSJU6 September 2020 TPS65982DMC
PRODUCTION DATA
The SPI master provides a serial interface to an external flash memory. The recommended memory is the W25Q80DV 8 Mbit Serial Flash Memory. A memory of at least 2 Mbit is required when the TPS65982DMC is using the memory in an unshared manner. A memory of at least 8 Mbit is required when the TPS65982DMC is using the memory in an shared manner. See theSPI Master Interface section for more information.