JAJSM58 June 2021 TPS65994AE
PRODUCTION DATA
The TUSB1046 requires GPIO control in GPIO control mode to determine whether if there is USB or DisplayPort data connection. Table 9-6 summarizes the TPS65994AE GPIO Events and the control pins for the TUSB1046. Note that the pin strapping on the TUSB1046 will set the GPIO control mode and the required equalizer settings. For more details refer to the TUSB1046 datasheet.
TPS65994AE GPIO EVENT | TUSB1046 CONTROL |
---|---|
Cable_Orientation_Event_Port1 | FLIP |
USB3_Event_Port1 | CTL0 |
DP_Mode_Selection_Event_Port1 | CTL1 |