DLPU082B August 2021 – August 2022 DLPC7540
A separate GPIO line (GPIO 58 by default) reports to the host component that the controller is busy or not busy. Upon power-on-reset, the front-end communication device must wait until the signal goes to LOW state. A signal that remains HIGH continuously indicates a problem with controller boot-sequence. The source of the problem must be resolve before proceeding.
When a command is sent, the I2C Busy GPIO is pulled HIGH until the command completes execution. If the device attempts to send another command while execution of the first command is ongoing, system confirms whether the I2C Busy GPIO is HIGH or LOW and then takes the decision to send the command. This process ensures that there is no clock stretching, and other devices on the I2C bus are not affected, but it ensures that the command handler is occupied and no other command can be sent at this point. Use the DLP Composer tool to assign a GPIO for this purpose.