JAJSG16 August 2018 PGA305
PRODUCTION DATA.
When configured in this mode, the FB– pin must be connected to the OUT pin. If the OUT pin is driving a large capacitive load, a compensation capacitor can be connected to the COMP pin and an isolation resistor can be placed between the OUT and FB– pins. The FB+ pin is not used in voltage mode.