JAJSG16 August 2018 PGA305
PRODUCTION DATA.
Data is transmitted on the one-wire interface in byte-sized packets. The first bit of the OWI field is the start bit. The next eight bits of the field are data bits to be processed by the OWI control logic. The final bit in the OWI field is the stop bit. A group of fields make up a transmission frame. A transmission frame is composed of the fields necessary to complete one transmission operation on the one-wire interface. The standard field structure for a one-wire field is shown in Figure 9.