JAJSGB9B January 2010 – October 2018 TLV320DAC3101
PRODUCTION DATA.
The requires multiple power supply rails for operation. All the power rails must be powered up for the device to operate at the fullest potention. The following is the recommended power-up sequencing for proper operation:
Although not necessary, if the system requires, during shutdown, remove the power supplies in the reverse order of the above sequence.