SLAAEF5B March 2024 – June 2025 MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3506 , MSPM0G3507 , MSPM0H3216 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1
Here is the test based on a 3800mAh LiFePO4 battery, under 25°C. u16MaxFullChgVoltThd setting is 3800mV. EmptyDhgVoltThd setting is 2300mV.
Here is the test pattern: do a pulse discharge 2 times. Figure 5-14 shows the condition of a battery Cell in the battery pack. Due to sourcemeter power limitations, only simple tests are run.
Figure 5-14 Battery TestcaseAt the beginning, there are obvious gaps for NomSOC, CusSOC and SmoothSOC. See the test results in Figure 5-14. This is caused from the first OCV calibration error. The reason why this is so high is that the calibration point is under the LiFePO4 SOC-OCV flat area.
Here are the results for one cell. With the integrated digital filter, the NomSOC changes follow the real condition even in first discharge cycle. However, as the current load is only 1A, users cannot see much influence of EmptySOC in CusSOC.
Figure 5-15 Battery Cell Test
ResultHere is the result for the battery pack,PackSOC, which follows the minimum SmoothSOC of all the Cells in the battery pack. PackFullCap is the combination of all the CusFullCap values, which are influenced by EmptySOC and FullSOC. That is why the data jumps in the PackFullCap chart. This is the same for PackRemCap, which is the combination of all the CusRemCap.
Figure 5-16 Battery Pack Test
Result