SLAAEF5B March 2024 – June 2025 MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3506 , MSPM0G3507 , MSPM0H3216 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1
This implementation is used to show the setup between MSPM0L1306 and BQ76905 with a setup of 5 cells to accelerate the evaluation speed on typical BQ devices. Unlike with BQ76952, BQ76905 does not have the passive equalization function, which needs to be implemented by users themselves.
Here is the hardware connection:
| LP-MSPM0L1306 | BQ76905 EVM | |
|---|---|---|
| GND | J7-1 | J4-1 |
| SCL | PA1 | J4-2 |
| SDA | PA0 | J4-3 |
Here is the real setup picture. Remember to short CELL5 to CELL4 and CELL3 to CELL2 cell input terminals before doing the evaluation.
Figure 5-20 Hardware Setup