SLAU367P October 2012 – April 2020 MSP430FR5041 , MSP430FR5043 , MSP430FR50431 , MSP430FR5847 , MSP430FR58471 , MSP430FR5848 , MSP430FR5849 , MSP430FR5857 , MSP430FR5858 , MSP430FR5859 , MSP430FR5867 , MSP430FR58671 , MSP430FR5868 , MSP430FR5869 , MSP430FR5870 , MSP430FR5872 , MSP430FR58721 , MSP430FR5887 , MSP430FR5888 , MSP430FR5889 , MSP430FR58891 , MSP430FR5922 , MSP430FR59221 , MSP430FR5947 , MSP430FR59471 , MSP430FR5948 , MSP430FR5949 , MSP430FR5957 , MSP430FR5958 , MSP430FR5959 , MSP430FR5962 , MSP430FR5964 , MSP430FR5967 , MSP430FR5968 , MSP430FR5969 , MSP430FR5969-SP , MSP430FR59691 , MSP430FR5970 , MSP430FR5972 , MSP430FR59721 , MSP430FR5986 , MSP430FR5987 , MSP430FR5988 , MSP430FR5989 , MSP430FR5989-EP , MSP430FR59891 , MSP430FR5992 , MSP430FR5994 , MSP430FR59941 , MSP430FR6005 , MSP430FR6007 , MSP430FR6035 , MSP430FR6037 , MSP430FR60371 , MSP430FR6041 , MSP430FR6043 , MSP430FR60431 , MSP430FR6045 , MSP430FR6047 , MSP430FR60471 , MSP430FR6820 , MSP430FR6822 , MSP430FR68221 , MSP430FR6870 , MSP430FR6872 , MSP430FR68721 , MSP430FR6877 , MSP430FR6879 , MSP430FR68791 , MSP430FR6887 , MSP430FR6888 , MSP430FR6889 , MSP430FR68891 , MSP430FR6920 , MSP430FR6922 , MSP430FR69221 , MSP430FR6927 , MSP430FR69271 , MSP430FR6928 , MSP430FR6970 , MSP430FR6972 , MSP430FR69721 , MSP430FR6977 , MSP430FR6979 , MSP430FR69791 , MSP430FR6987 , MSP430FR6988 , MSP430FR6989 , MSP430FR69891
Receive timing error consists of two error sources. The first is the bit-to-bit timing error similar to the transmit bit timing error. The second is the error between a start edge occurring and the start edge being accepted by the eUSCI_A module. Figure 30-11 shows the asynchronous timing errors between data on the UCAxRXD pin and the internal baud-rate clock. This results in an additional synchronization error. The synchronization error tSYNC is between –0.5 BRCLKs and +0.5 RCLKs, independent of the selected baud-rate generation mode.
Figure 30-11 Receive Error The ideal sampling time tbit,ideal,RX[i] is in the middle of a bit period:
tbit,ideal,RX[i] = (1/baud rate)(i + 0.5)
The real sampling time, tbit,RX[i], is equal to the sum of all previous bits according to the formulas shown in the transmit timing section, plus one-half BITCLK for the current bit i, plus the synchronization error tSYNC.
This results in the following tbit,RX[i] for the low-frequency baud-rate mode:
Where:
Tbit,RX[i] = (1/fBRCLK)(UCBRx + mUCBRSx[i])
mUCBRSx[i] = Modulation of bit i of UCBRSx
For the oversampling baud-rate mode, the sampling time tbit,RX[i] of bit i is calculated by:
Where:
= Sum of ones from columns 0 to (7 + mUCBRSx[i]) from the corresponding row in Table 30-3.
mUCBRSx[i] = Modulation of bit i of UCBRSx
This results in an error normalized to one ideal bit time (1/baud rate) according to the following formula:
ErrorRX[i] = (tbit,RX[i] – tbit,ideal,RX[i]) × baud rate × 100%