SLAU367P October 2012 – April 2020 MSP430FR5041 , MSP430FR5043 , MSP430FR50431 , MSP430FR5847 , MSP430FR58471 , MSP430FR5848 , MSP430FR5849 , MSP430FR5857 , MSP430FR5858 , MSP430FR5859 , MSP430FR5867 , MSP430FR58671 , MSP430FR5868 , MSP430FR5869 , MSP430FR5870 , MSP430FR5872 , MSP430FR58721 , MSP430FR5887 , MSP430FR5888 , MSP430FR5889 , MSP430FR58891 , MSP430FR5922 , MSP430FR59221 , MSP430FR5947 , MSP430FR59471 , MSP430FR5948 , MSP430FR5949 , MSP430FR5957 , MSP430FR5958 , MSP430FR5959 , MSP430FR5962 , MSP430FR5964 , MSP430FR5967 , MSP430FR5968 , MSP430FR5969 , MSP430FR5969-SP , MSP430FR59691 , MSP430FR5970 , MSP430FR5972 , MSP430FR59721 , MSP430FR5986 , MSP430FR5987 , MSP430FR5988 , MSP430FR5989 , MSP430FR5989-EP , MSP430FR59891 , MSP430FR5992 , MSP430FR5994 , MSP430FR59941 , MSP430FR6005 , MSP430FR6007 , MSP430FR6035 , MSP430FR6037 , MSP430FR60371 , MSP430FR6041 , MSP430FR6043 , MSP430FR60431 , MSP430FR6045 , MSP430FR6047 , MSP430FR60471 , MSP430FR6820 , MSP430FR6822 , MSP430FR68221 , MSP430FR6870 , MSP430FR6872 , MSP430FR68721 , MSP430FR6877 , MSP430FR6879 , MSP430FR68791 , MSP430FR6887 , MSP430FR6888 , MSP430FR6889 , MSP430FR68891 , MSP430FR6920 , MSP430FR6922 , MSP430FR69221 , MSP430FR6927 , MSP430FR69271 , MSP430FR6928 , MSP430FR6970 , MSP430FR6972 , MSP430FR69721 , MSP430FR6977 , MSP430FR6979 , MSP430FR69791 , MSP430FR6987 , MSP430FR6988 , MSP430FR6989 , MSP430FR69891
The 16-bit status register (SR, also called R2), used as a source or destination register, can only be used in register mode addressed with word instructions. The remaining combinations of addressing modes are used to support the constant generator. Figure 4-9 shows the SR bits. Do not write 20-bit values to the SR. Unpredictable operation can result.
Figure 4-9 SR Bits Table 4-1 describes the SR bits.
| Bit | Description | |
|---|---|---|
| Reserved | Reserved | |
| V | Overflow. This bit is set when the result of an arithmetic operation overflows the signed-variable range. | |
ADD(.B), ADDX(.B,.A),
ADDC(.B), ADDCX(.B.A),
ADDA
|
Set when:
positive + positive = negative negative + negative = positive otherwise reset |
|
SUB(.B), SUBX(.B,.A),
SUBC(.B),SUBCX(.B,.A),
SUBA, CMP(.B),
CMPX(.B,.A), CMPA
|
Set when:
positive – negative = negative negative – positive = positive otherwise reset |
|
| SCG1 | System clock generator 1. This bit may be used to enable or disable functions in the clock system depending on the device family; for example, DCO bias enable or disable. | |
| SCG0 | System clock generator 0. This bit may be used to enable or disable functions in the clock system depending on the device family; for example, FLL enable or disable. | |
| OSCOFF | Oscillator off. When this bit is set, it turns off the LFXT1 crystal oscillator when LFXT1CLK is not used for MCLK or SMCLK. In FRAM devices, CPUOFF must be 1 to disable the cyrstal oscillator. | |
| CPUOFF | CPU off. When this bit is set, it turns off the CPU and requests a low-power mode according to the settings of bits OSCOFF, SCG0, and SCG1. | |
| GIE | General interrupt enable. When this bit is set, it enables maskable interrupts. When it is reset, all maskable interrupts are disabled. | |
| N | Negative. This bit is set when the result of an operation is negative and cleared when the result is positive. | |
| Z | Zero. This bit is set when the result of an operation is 0 and cleared when the result is not 0. | |
| C | Carry. This bit is set when the result of an operation produced a carry and cleared when no carry occurred. | |
NOTE
Bit manipulations of the SR should be done by the following instructions: MOV, BIS, and BIC.