SLUAB06 January 2025 AMC131M02 , AMC3330 , ISO7731
The Y capacitance in insulation testing has a great influence on the speed of insulation testing. The mechanism of the Y capacitance affecting insulation detection is, for example, in the bridge method, that it delays the time of steady state establishment, if the unconverged voltage value is used to calculate, The resulting insulation resistance value is also inaccurate.