SLVAF66 June   2021 DRV3255-Q1 , DRV8300 , DRV8301 , DRV8302 , DRV8303 , DRV8304 , DRV8305 , DRV8305-Q1 , DRV8306 , DRV8307 , DRV8308 , DRV8320 , DRV8320R , DRV8323 , DRV8323R , DRV8340-Q1 , DRV8343-Q1 , DRV8350 , DRV8350F , DRV8350R , DRV8353 , DRV8353F , DRV8353R

 

  1. 1 Introduction to High-Power Motor Applications
    1. 1.1 Effects of a Poorly-Designed High-Power Motor Driver System
    2. 1.2 Example of the High-Power Design Process
  2. 2 Examining a High-Power Motor Drive System at a High Level
    1. 2.1 Anatomy of the Motor Drive Power Stage and How to Troubleshoot
    2. 2.2 Troubleshooting a High-Power System
  3. 3 High-Power Design Through MOSFETs and MOSFET Gate Current (IDRIVE)
    1. 3.1 MOSFET Gate Current
      1. 3.1.1 How Gate Current Causes Damage
      2. 3.1.2 Gate Resistors and Smart Gate Drive Technology
        1. 3.1.2.1 Gate Resistors
        2. 3.1.2.2 Smart Gate Drive and Internally-Controlled Sink and Source Gate Currents
        3. 3.1.2.3 Summary for Gate Resistors and Smart Gate Drive Technology
      3. 3.1.3 Example Gate Current Calculation for a Given FET
  4. 4 High-Power Design Through External Components
    1. 4.1 Bulk and Decoupling Capacitors
      1. 4.1.1 Note on Capacitor Voltage Ratings
    2. 4.2 RC Snubber Circuits
    3. 4.3 High-Side Drain to Low-Side Source Capacitor
    4. 4.4 Gate-to-GND Diodes
  5. 5 High-Power Design Through a Parallel MOSFET Power Stage
  6. 6 High-Power Design Through Protection
    1. 6.1 VDS and VGS Monitoring
      1. 6.1.1 Turning Off the FETs During an Overcurrent, Shoot-Through, or FET Shorting Event
    2. 6.2 Passive Gate-to-Source Pulldown Resistors
    3. 6.3 Power Supply Reverse Polarity or Power Supply Cutoff Protection
  7. 7 High-Power Design Through Motor Control Methods
    1. 7.1 Brake versus Coast
      1. 7.1.1 Algorithm-Based Solutions
      2. 7.1.2 External Circuit Solutions
      3. 7.1.3 Summary of Brake versus Coast
  8. 8 High-Power Design Through Layout
    1. 8.1 What is a Kelvin Connection?
    2. 8.2 General Layout Advice
  9. 9 Conclusion
  10. 10Acknowledgments

Brake versus Coast

Figure 7-1 Example of Current Flowing Through Body Diodes During Coast Condition

Stopping or coasting a rotor already in motion is a typical use case that can cause problems for a high-power design. In this specific definition, coasting is when all of the high and low sides are turned off, which can be understood as floating the motor phases. Motors are partially inductive loads, so inductors attempt to resist changes in current by producing voltage to maintain current to flow in addition to the back EMF generated from the magnetic material of the rotor passing by the stator coils. As a result, the voltage at the motor phase rises higher than the voltage seen at the drain of the FET, which causes current to flow from the motor, through the body diodes of the FETs and into the supply over time during this coasting condition.

These spikes in voltage and the increased current out of the motor phases goes into the supply and increases the equivalent voltage at the FET drain to a higher value. As mentioned previously, the bulk capacitors absorb some or all of this energy, but the resulting rise in voltage can easily exceed absolute maximums for the gate driver if left unchecked as the bulk capacitors increase in voltage.

This actually occurs during the dead time of every PWM cycle, but the FETs stay in the coast state for such a short amount of time that the resulting energy usually does not move to the supply fast enough to cause damage. However, the increased voltage on the high-side source can be detected.

Luckily, this is avoided through motor control methods or external circuits, and the best practice is to have a plan to manage the energy stored up in the coils. Instead of coasting, implementing a braking control method or adding an external circuit is preferred.