SPNU151W January 1998 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , OMAP-L132 , OMAP-L137 , OMAP-L138 , SM470R1B1M-HT , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
Options control the operation of the compiler. This section provides a description of option conventions and an option summary table. It also provides detailed descriptions of the most frequently used options, including options used for type-checking and assembling.
For a help screen summary of the options, enter armcl with no parameters on the command line.
The following apply to the compiler options:
You can define default options for the compiler by using the TI_ARM_C_OPTION environment variable. For a detailed description of the environment variable, see Section 2.4.1.
Table 2-1 through Table 2-29 summarize all options (including link options). Use the references in the tables for more complete descriptions of the options.
| Option | Alias | Effect | Section |
|---|---|---|---|
| --silicon_version={ 4 | 5e | 6 | 6M0 | 7A8 | 7M3 | 7M4 | 7R4 | 7R5 } | -mv | Selects processor version: ARM V4 (ARM7), ARM V5e (ARM9E), ARM V6 (ARM11), ARM V6M0 (Cortex-M0), ARM V7A8 (Cortex-A8), ARM V7M3 (Cortex-M3), ARM V7M4 (Cortex-M4), ARM V7R4 (Cortex-R4), or ARM V7R5 (Cortex-R5). The default is ARM V4. | Section 2.3.4 |
| --code_state={ 16 | 32 } | Designates the ARM compilation mode. | Section 2.3.4 | |
| --float_support={ vfpv2 | vfpv3 | vfpv3d16 | fpv4spd16 | none ) | Generates vector floating-point (VFP) coprocessor instructions. Use this option only if the target hardware provides this functionality. | Section 2.14 | |
| --little_endian or --endian={ big | little } | -me | Designates little-endian code. The default is big-endian. | Section 2.3.4 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --opt_level=off | Disables all optimization. | Section 3.1 | |
| --opt_level=n | -On | Level 0 (-O0) optimizes
register usage only. Level 1 (-O1) uses Level 0 optimizations and optimizes locally. Level 2 (-O2) uses Level 1 optimizations and optimizes globally. Level 3 (-O3) uses Level 2 optimizations and optimizes the file (default if option not used). Level 4 (-O4) uses Level 3 optimizations and performs link-time optimization. |
Section 3.1, Section 3.3, Section 3.6 |
| --opt_for_speed[=n] | -mf | Controls the tradeoff between size and speed (0-5 range). If this option is specified without n, the default value is 4. If this option is not specified, the default setting is 1. | Section 3.2 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --auto_inline=[size] | -oi | Sets automatic inlining size (--opt_level=3 only). If size is not specified, the default is 1. | Section 3.5 |
| --call_assumptions=n | -opn | Level 0 (-op0) specifies
that the module contains functions and variables that are called or
modified from outside the source code provided to the compiler. Level 1 (-op1) specifies that the module contains variables modified from outside the source code provided to the compiler but does not use functions called from outside the source code. Level 2 (-op2) specifies that the module contains no functions or variables that are called or modified from outside the source code provided to the compiler (default). Level 3 (-op3) specifies that the module contains functions that are called from outside the source code provided to the compiler but does not use variables modified from outside the source code. |
Section 3.4.1 |
| --disable_inlining | Prevents any inlining from occurring. | Section 2.11 | |
| --fp_mode={relaxed|strict} | Enables or disables relaxed floating-point mode. | Section 2.3.3 | |
| --fp_reassoc={on|off} | Enables or disables the reassociation of floating-point arithmetic. | Section 2.3.3 | |
| --gen_opt_info=n | -onn | Level 0 (-on0) disables the
optimization information file. Level 1 (-on2) produces an optimization information file. Level 2 (-on2) produces a verbose optimization information file. |
Section 3.3.1 |
| --optimizer_interlist | -os | Interlists optimizer comments with assembly statements. | Section 3.11 |
| --program_level_compile | -pm | Combines source files to perform program-level optimization. | Section 3.4 |
| --sat_reassoc={on|off} | Enables or disables the reassociation of saturating arithmetic. Default is --sat_reassoc=off. | Section 2.3.3 | |
| --aliased_variables | -ma | Indicates that a specific aliasing technique is used. | Section 3.9 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --symdebug:dwarf | -g | Default behavior. Enables symbolic debugging. The generation of debug information does not impact optimization. Therefore, generating debug information is enabled by default. | Section 2.3.5
Section 3.12 |
| --symdebug:dwarf_version=2|3|4 | Specifies the DWARF format version. | Section 2.3.5 | |
| --symdebug:none | Disables all symbolic debugging. | Section 2.3.5 Section 3.12 |
|
| --symdebug:skeletal | (Deprecated; has no effect.) |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --include_path=directory | -I |
Adds the specified directory to the #include search path. | Section 2.5.2.1 |
| --preinclude=filename | Includes filename at the beginning of compilation. | Section 2.3.3 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --advice:power[={all|none|rulespec}] | Enables checking the specified ULP Advisor rules. (Default is all.) | Section 2.3.3 | |
| --advice:power_severity={error| warning|remark|suppress} |
Sets the diagnostic severity for ULP Advisor rules. | Section 2.3.3 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --compile_only | -c | Disables linking (negates --run_linker). | Section 4.1.3 |
| --help | -h | Prints (on the standard output device) a description of the options understood by the compiler. | Section 2.3.2 |
| --run_linker | -z | Causes the linker to be invoked from the compiler command line. | Section 2.3.2 |
| --skip_assembler | -n | Compiles C/C++ source file , producing an assembly language output file. The assembler is not run and no object file is produced. | Section 2.3.2 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --c89 | Processes C files according to the ISO C89 standard. | Section 5.16 | |
| --c99 | Processes C files according to the ISO C99 standard. | Section 5.16 | |
| --c11 | Processes C files according to the ISO C11 standard. | Section 5.16 | |
| --c++14 | Processes C++ files according to the ISO C++14 standard. The --c++03 option has been deprecated. |
Section 5.16 | |
| --cpp_default | -fg | Processes all source files with a C extension as C++ source files. | Section 2.3.7 |
| --enum_type={int|packed} | Choose whether to use compact integer types to store small enumerated types. | Section 2.3.4 | |
| --exceptions | Enables C++ exception handling. | Section 5.8 | |
| --extern_c_can_throw | Allow extern C functions to propagate exceptions. | -- | |
| --float_operations_allowed ={none|all|32|64} |
Restricts the types of floating point operations allowed. | Section 2.3.3 | |
| --gen_cross_reference_listing | -px | Generates a cross-reference listing file (.crl). | Section 2.9 |
| --pending_instantiations=# | Specify the number of template instantiations that may be in progress at any given time. Use 0 to specify an unlimited number. | Section 2.3.4 | |
| --plain_char={signed|unsigned} | -mc | Specifies how to treat plain chars, default is unsigned. | Section 2.3.4 |
| --printf_support={nofloat|full| minimal} |
Enables support for smaller, limited versions of the printf function family (sprintf, fprintf, etc.) and the scanf function family (sscanf, fscanf, etc.) run-time-support functions. | Section 2.3.3 | |
| --relaxed_ansi | -pr | Enables relaxed mode; ignores strict ISO violations. This is on by default. To disable this mode, use the --strict_ansi option. | Section 5.16.3 |
| --rtti | -rtti | Enables C++ run-time type information (RTTI). | –- |
| --strict_ansi | -ps | Enables strict ANSI/ISO mode (for C/C++, not for K&R C). In this mode, language extensions that conflict with ANSI/ISO C/C++ are disabled. In strict ANSI/ISO mode, most ANSI/ISO violations are reported as errors. Violations that are considered discretionary may be reported as warnings instead. | Section 5.16.3 |
| --wchar_t={32|16} | Sets the size of the C/C++ type wchar_t. Default is 16 bits. | Section 2.3.4 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --preproc_dependency[=filename] | -ppd | Performs preprocessing only, but instead of writing preprocessed output, writes a list of dependency lines suitable for input to a standard make utility. | Section 2.5.8 |
| --preproc_includes[=filename] | -ppi | Performs preprocessing only, but instead of writing preprocessed output, writes a list of files included with the #include directive. | Section 2.5.9 |
| --preproc_macros[=filename] | -ppm | Performs preprocessing only. Writes list of predefined and user-defined macros to a file with the same name as the input but with a .pp extension. | Section 2.5.10 |
| --preproc_only | -ppo | Performs preprocessing only. Writes preprocessed output to a file with the same name as the input but with a .pp extension. | Section 2.5.4 |
| --preproc_with_comment | -ppc | Performs preprocessing only. Writes preprocessed output, keeping the comments, to a file with the same name as the input but with a .pp extension. | Section 2.5.6 |
| --preproc_with_compile | -ppa | Continues compilation after preprocessing with any of the -pp<x> options that normally disable compilation. | Section 2.5.5 |
| --preproc_with_line | -ppl | Performs preprocessing only. Writes preprocessed output with line-control information (#line directives) to a file with the same name as the input but with a .pp extension. | Section 2.5.7 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --define=name[=def] | -D | Predefines name. | Section 2.3.2 |
| --undefine=name | -U | Undefines name. | Section 2.3.2 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --compiler_revision | Prints out the compiler release revision and exits. | -- | |
| --diag_error=num | -pdse | Categorizes the diagnostic identified by num as an error. | Section 2.7.1 |
| --diag_remark=num | -pdsr | Categorizes the diagnostic identified by num as a remark. | Section 2.7.1 |
| --diag_suppress=num | -pds | Suppresses the diagnostic identified by num. | Section 2.7.1 |
| --diag_warning=num | -pdsw | Categorizes the diagnostic identified by num as a warning. | Section 2.7.1 |
| --diag_wrap={on|off} | Wrap diagnostic messages (default is on). Note that this command-line option cannot be used within the Code Composer Studio IDE. | ||
| --display_error_number | -pden | Displays a diagnostic's identifiers along with its text. Note that this command-line option cannot be used within the Code Composer Studio IDE. | Section 2.7.1 |
| --emit_warnings_as_errors | -pdew | Treat warnings as errors. | Section 2.7.1 |
| --gen_func_info_listing | Generate user information file (.aux). | Section 2.3.2 | |
| --issue_remarks | -pdr | Issues remarks (non-serious warnings). | Section 2.7.1 |
| --no_warnings | -pdw | Suppresses diagnostic warnings (errors are still issued). | Section 2.7.1 |
| --quiet | -q | Suppresses progress messages (quiet). | -- |
| --set_error_limit=num | -pdel | Sets the error limit to num. The compiler abandons compiling after this number of errors. (The default is 100.) | Section 2.7.1 |
| --super_quiet | Super quiet mode. | -- | |
| --tool_version | -version | Displays version number for each tool. | -- |
| --verbose | Display banner and function progress information. | -- | |
| --verbose_diagnostics | -pdv | Provides verbose diagnostic messages that display the original source with line-wrap. Note that this command-line option cannot be used within the Code Composer Studio IDE. | Section 2.7.1 |
| --write_diagnostics_file | Generates a diagnostic message information file. Compiler only option. Note that this command-line option cannot be used within the Code Composer Studio IDE. | Section 2.7.1 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --gen_preprocessor_listing | -pl | Generates a raw listing file (.rl). | Section 2.10 |
| --section_sizes={on|off} | Generates section size information, including sizes for sections containing executable code and constants, constant or initialized data (global and static variables), and uninitialized data. (Default is off if this option is not included on the command line. Default is on if this option is used with no value specified.) | Section 2.7.1 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --common={on|off} | On by default. When on, uninitialized file scope variables are emitted as common symbols. When off, common symbols are not created. | Section 2.3.4 | |
| --embedded_constants={on|off} | Controls whether compiler embeds constants in functions. | Section 2.3.4 | |
| --gen_data_subsections={on|off} | Place all aggregate data (arrays, structs, and unions) into subsections. This gives the linker more control over removing unused data during the final link step. See the link to the right for details about the default setting. | Section 4.2.2 | |
| --global_register={r5|r6|r9} | -rr | Disallows use of rx=[5,6,9] by the compiler. | Section 2.3.4 |
| -neon | Enables support for the Cortex-A8 Neon SIMD instruction set. | Section 2.3.4 | |
| --ramfunc={on|off} | If set to on, specifies that all functions should be placed in the .TI.ramfunc section, which is placed in RAM. | Section 2.3.4 | |
| --unaligned_access={on|off} | Controls generation of unaligned accesses. | Section 2.3.4 | |
| --use_dead_funcs_list [=fname] | Places each function listed in the file in a separate section. | Section 2.3.4 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --entry_hook[=name] | Enables entry hooks. | Section 2.15 | |
| --entry_parm={none|name| address} |
Specifies the parameters to the function to the --entry_hook option. | Section 2.15 | |
| --exit_hook[=name] | Enables exit hooks. | Section 2.15 | |
| --exit_parm={none|name|address} | Specifies the parameters to the function to the --exit_hook option. | Section 2.15 | |
| --remove_hooks_when_inlining | Removes entry/exit hooks for auto-inlined functions. | Section 2.15 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --analyze=codecov | Generate analysis info from profile data. | Section 3.8.2.2 | |
| --analyze_only | Only generate analysis. | Section 3.8.2.2 | |
| --gen_profile_info | Generates instrumentation code to collect profile information. | Section 3.7.1.3 | |
| --use_profile_info=file1[, file2,...] | Specifies the profile information file(s). | Section 3.7.1.3 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --keep_asm | -k | Keeps the assembly language (.asm) file. | Section 2.3.11 |
| --asm_listing | -al | Generates an assembly listing file. | Section 2.3.11 |
| --c_src_interlist | -ss | Interlists C source and assembly statements. | Section 2.12
Section 3.11 |
| --src_interlist | -s | Interlists optimizer comments (if available) and assembly source statements; otherwise interlists C and assembly source statements. | Section 2.3.2 |
| --absolute_listing | -aa | Enables absolute listing. | Section 2.3.11 |
| --asm_cross_reference_listing | -ax | Generates the cross-reference file. | Section 2.3.11 |
| --asm_define=name[=def] | -ad | Sets the name symbol. | Section 2.3.11 |
| --asm_dependency | -apd | Performs preprocessing; lists only assembly dependencies. | Section 2.3.11 |
| --asm_includes | -api | Performs preprocessing; lists only included #include files. | Section 2.3.11 |
| --asm_undefine=name | -au | Undefines the predefined constant name. | Section 2.3.11 |
| --code_state={16|32} | Begins assembling instructions as 16- or 32-bit instructions. | Section 2.3.11 | |
| --include_file=filename | -ahi | Includes the specified file for the assembly module. | Section 2.3.11 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --asm_file=filename | -fa | Identifies filename as an assembly source file regardless of its extension. By default, the compiler and assembler treat .asm files as assembly source files. | Section 2.3.7 |
| --c_file=filename | -fc | Identifies filename as a C source file regardless of its extension. By default, the compiler treats .c files as C source files. | Section 2.3.7 |
| --cpp_file=filename | -fp | Identifies filename as a C++ file, regardless of its extension. By default, the compiler treats .C, .cpp, .cc and .cxx files as a C++ files. | Section 2.3.7 |
| --obj_file=filename | -fo | Identifies filename as an object code file regardless of its extension. By default, the compiler and linker treat .obj files as object code files, including both *.c.obj and *.cpp.obj files. | Section 2.3.7 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --abs_directory=directory | -fb | Specifies an absolute listing file directory. By default, the compiler uses the object file directory. | Section 2.3.10 |
| --asm_directory=directory | -fs | Specifies an assembly file directory. By default, the compiler uses the current directory. | Section 2.3.10 |
| --list_directory=directory | -ff | Specifies an assembly listing file and cross-reference listing file directory By default, the compiler uses the object file directory. | Section 2.3.10 |
| --obj_directory=directory | -fr | Specifies an object file directory. By default, the compiler uses the current directory. | Section 2.3.10 |
| --output_file=filename | -fe | Specifies a compilation output file name; can override --obj_directory. | Section 2.3.10 |
| --pp_directory=dir | Specifies a preprocessor file directory. By default, the compiler uses the current directory. | Section 2.3.10 | |
| --temp_directory=directory | -ft | Specifies a temporary file directory. By default, the compiler uses the current directory. | Section 2.3.10 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --asm_extension=[.]extension | -ea | Sets a default extension for assembly source files. | Section 2.3.9 |
| --c_extension=[.]extension | -ec | Sets a default extension for C source files. | Section 2.3.9 |
| --cpp_extension=[.]extension | -ep | Sets a default extension for C++ source files. | Section 2.3.9 |
| --listing_extension=[.]extension | -es | Sets a default extension for listing files. | Section 2.3.9 |
| --obj_extension=[.]extension | -eo | Sets a default extension for object files. | Section 2.3.9 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --cmd_file=filename | -@ | Interprets contents of a file as an extension to the command line. Multiple -@ instances can be used. | Section 2.3.2 |
| Option | Alias | Effect | Section |
|---|---|---|---|
| --check_misra[={all|required| advisory|none|rulespec}] |
Enables checking of the specified MISRA-C:2004 rules. Default is all. | Section 2.3.3 | |
| --misra_advisory={error|warning| remark|suppress} |
Sets the diagnostic severity for advisory MISRA-C:2004 rules. | Section 2.3.3 | |
| --misra_required={error|warning| remark|suppress} |
Sets the diagnostic severity for required MISRA-C:2004 rules. | Section 2.3.3 |