SPRACM3E August 2021 – January 2023 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The star topology over FSI application example demonstrates a different kind of communication topology, showcasing how a central host device can receive information from multiple node devices at the same time rather than wait for packets to be forwarded through subsequent devices, like in the daisy-chain example. The advantages and disadvantages of the star topology are discussed in Section 2.
The defining requirements of the star implementation provided are hardware related, i.e. host device TX needing to have multi-drop functionality to each node, and MCU resource related, i.e. host device needing N number of RX instances. From a software perspective the central host device uses a new star_broadcast project while the N node devices use the same node device software utilized in the daisy-chain tests, details provided in Table 6-1.
Project | Description | Supported Devices |
---|---|---|
fsi_ex_star_broadcast | Project for central host device in the star network | F2838x |
fsi_ex_daisy_handshake_node | Project for N number of node devices in the star network | F28002x, F28004x, F2838x |
The software flow of the star_broadcast project is similar to that of the lead device CPU Control daisy-chain project discussed in Section 5. The handshake mechanism is slightly different as shown in Section 3.2. Upon completion of the handshake, the central host device transmits a broadcast data frame to all of the node devices connected to its FSITX. The host then waits to receive the data frame back from all connected node devices and then validates that each received frame matches the originally transmitted one, after which it prepares and sends a new data frame.
By default, the star_broadcast project has pre-made configurations for FSI RX instances A, B and C of the device. Each instance can be configured by setting the individual pre-processor directives below to "1". Additional FSI RX instances can be added if they are available on the host device.
//
// Enable FSI RX Instances
//
#define FSI_RXA_ENABLE 1
#define FSI_RXB_ENABLE 0
#define FSI_RXC_ENABLE 1
Timing measurements of the star topology are very similar, if not the same, as those collected in the previous daisy-chain tests. Therefore, the data provided in Table 5-4 can be utilized for this purpose.