High-speed (HS) bypass capacitors are critical for
proper DDR interface operation. This is particularly important to minimize the
parasitic series inductance of the HS bypass capacitors to VDDS_DDR and the
associated ground connections. Table 1-3 contains the specification for the HS bypass capacitors and for the power
connections on the PCB. Generally speaking, TI recommends:
- Fitting as many HS bypass capacitors as possible.
- Minimizing the distance from the bypass capacitor to the pins and balls being bypassed.
- Using the smallest physical sized ceramic capacitors possible with the highest capacitance readily available.
- Connecting the bypass capacitor pads to the vias using the widest traces
possible and using the largest via hole size possible.
- Minimizing via sharing. Note the limits on via sharing shown in Table 1-3.
- Using three-terminal capacitors
instead of two terminal capacitors. Three-terminal capacitors provide lower loop
inductance, and one three-terminal capacitor can take the place of multiple
two-terminal capacitors, further optimizing loop inductance.
For any additional SDRAM requirements, see the manufacturer's data sheet.
Table 1-3 High-Speed Bypass
Capacitors
| Parameter |
MIN |
TYP |
MAX |
UNIT |
| HS bypass capacitor package size (1) |
|
0201 |
0402 |
Mils |
| Distance, HS bypass capacitor to processor being bypassed (2)(3)(4) |
|
|
150 |
Mils |
| Processor HS bypass capacitor count per VDDS_DDR rail(5) |
5 |
|
|
Devices |
| Processor HS bypass capacitor total capacitance per VDDS_DDR
rail(5) |
1.4 |
|
|
uF |
| Number of connection vias for each device power/ground
ball |
1 |
|
|
Vias |
| Trace length from processor power/ground ball to connection via
(2) |
|
35 |
70 |
Mils |
| Distance, HS bypass capacitor to DDR device being bypassed (6) |
|
|
150 |
Mils |
| DDR device HS bypass capacitor count |
Refer to DDR manufacturer
guidelines |
| Number of connection vias for each HS capacitor (7)(8) |
2 |
|
|
Vias |
| Trace length from bypass capacitor to connection via (2)(8) |
|
35 |
100 |
Mils |
| Number of connection vias for each DDR device power/ground
ball |
1 |
|
|
Vias |
| Trace length from DDR device power/ground ball to connection via
(2) |
|
35 |
60 |
Mils |
(1) LxW, 10-mil units, that is, a 0402 is a 40x20-mil surface-mount capacitor.
(2) Closer or shorter is preferable.
(3) Measured from the nearest processor power or ground ball to the center of the capacitor package.
(4) Three of these capacitors need to be located underneath the processor, among
the cluster of VDDS_DDR balls.
(5) Decoupling capacitor counts and
capacitor values need to be derived from power aware PCB simulations. The PCB
designer has a responsibility to make sure that any design meets the provided
PDN targets.
(6) Measured from the DDR device power or ground ball to the center of the capacitor package. Refer to the guidance from the SDRAM manufacturer.
(7) An additional HS bypass capacitor can share the connection vias only if the
bypass is mounted on the opposite side of the board. No sharing of vias is
permitted on the same side of the board.
(8) An HS bypass capacitor can share a via with a DDR device mounted on the same
side of the PCB. A wide trace must be used for the connection, and the length
from the capacitor pad to the DDR device pad needs to be less than 150
mils.