SPRUIY9C May   2021  – December 2025

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Device Information
  6. 2Hardware
    1. 2.1 EVM Revisions and Assembly Variants
    2. 2.2 Important Usage Notes
    3. 2.3 System Description
      1. 2.3.1 Functional Block Diagram
      2. 2.3.2 Power-On/Off Procedures
        1. 2.3.2.1 Power-On Procedure
        2. 2.3.2.2 Power-Off Procedure
      3. 2.3.3 Peripheral and Major Component Description
        1. 2.3.3.1  Clocking
          1. 2.3.3.1.1 Ethernet PHY Clock
          2. 2.3.3.1.2 AM64x SoC Clock
        2. 2.3.3.2  Reset
        3. 2.3.3.3  Power
          1. 2.3.3.3.1 Power Input
          2. 2.3.3.3.2 USB Type-C Interface for Power Input
          3. 2.3.3.3.3 Power Fault Indication
          4. 2.3.3.3.4 Power Supply
          5. 2.3.3.3.5 Power Sequencing
          6. 2.3.3.3.6 Power Supply
        4. 2.3.3.4  Configuration
          1. 2.3.3.4.1 Boot Modes
        5. 2.3.3.5  JTAG
        6. 2.3.3.6  Test Automation
        7. 2.3.3.7  UART Interface
        8. 2.3.3.8  Memory Interfaces
          1. 2.3.3.8.1 LPDDR4 Interface
          2. 2.3.3.8.2 MMC Interface
            1. 2.3.3.8.2.1 Micro SD Interface
            2. 2.3.3.8.2.2 WiLink Interface
            3. 2.3.3.8.2.3 OSPI Interface
            4. 2.3.3.8.2.4 Board ID EEPROM Interface
        9. 2.3.3.9  Ethernet Interface
          1. 2.3.3.9.1 DP83867 PHY Default Configuration
          2. 2.3.3.9.2 DP83867 – Power, Clock, Reset, Interrupt and LEDs
          3. 2.3.3.9.3 Industrial Application LEDs
        10. 2.3.3.10 USB 3.0 Interface
        11. 2.3.3.11 PRU Connector
        12. 2.3.3.12 User Expansion Connector
        13. 2.3.3.13 MCU Connector
        14. 2.3.3.14 Interrupt
        15. 2.3.3.15 I2C Interface
        16. 2.3.3.16 IO Expander (GPIOs)
  7. 3Hardware Design Files
  8. 4Compliance Information
    1. 4.1 Regulatory Compliance
  9. 5Additional Information
    1. 5.1 Known Issues
      1. 5.1.1 Issue 1: LP8733x Max output Capacitance Spec Exceeded on LDO0 and LDO1
      2. 5.1.2 Issue 2: LP8733x Output Voltage of 0.9V Exceeds AM64x VDDR_CORE max Voltage Spec of 0.895 V
      3. 5.1.3 Issue 3 - SDIO Devices on MMC0 Require Careful Trace Lengths to Meet Interface Timing Requirements
      4. 5.1.4 Issue 4 - LPDDR4 Data Rate Limitation in Stressful Conditions
      5. 5.1.5 Issue 5 - Junk Character
      6. 5.1.6 Issue 6 - Test Power Down Signal Floating
      7. 5.1.7 Issue 7 - uSD Boot Not Working
    2.     Trademarks
    3.     65
  10. 6Revision History

Test Automation

The SKEVM has a 40 pin test automation header (J16) to allow an external controller to manipulate some basic operations like Power Down, POR, Warm Reset, Boot Mode control, etc. The test automation header includes four GPIOs and two I2C interfaces (I2C1, Boot mode I2C0).

The test automation circuit has voltage translation circuits so that the controller is isolated from the IO voltages used by the AM64x. Boot mode for the AM64x must be controlled by either the user using DIP Switches or the test automation header through the I2C IO Expander.

Boot Mode Buffers are used to isolate the Boot Mode controls driven through DIP Switches or I2C IO Expanders. Power to Test Automation Circuit is provided from a Power Mux (TPS2121RUXT) which is having the input supplies VCC3V3_TA supply generated from a dedicated regulator and VCC3V3_XDS generated from an LDO (it is the supply for XDS110 Debugger section). The basic controls of test automation header J16 are as follows. Table 2-16 gives details about test automation header signals.

Optionally, the Test Automation header functionality can be implemented by the XDS110 controller. Hence resistor options (R420, R421, R422, R423, R424, R425, R426, R427, R436, R437, R438 and R439) are provided for Power Down, POR, Warm Reset, Boot Mode controls and GPIO signals. By default these resistors are made as DNI so that an external controller controls the basic operations through the Automation header. Once the firmware for the XDS110 is developed, then mount the above mentioned resistors and DNI the following resistors R380, R381, R382, R383, R384, R385, R386, R432, R433, R434 and R435 to control the basic operations through the XDS110 microcontroller.

Proper Isolation to be provided on Boot Mode signals to allow normal operation. SoC_I2C [1] connected to test automation header to communicate with external controller.

One of the I2C interfaces from Test automation header is connected to the Boot mode buffer to control the boot mode of AM64x and another I2C interface is connected to the I2C1 port of AM64x.

Table 2-16 lists the reset signals routed from test automation header. The boot mode for the AM64x can be controlled by either the user or the test automation header. The boot mode is controlled by the user using two separate 8-positions DIP switches on the board. The switches connect a pull-up resistor to the output of a buffer when the switch is set to ON position. When the switch is off, a weaker pull-down resistor holds the signal low. The output of the buffer is connected to the boot mode pins on the AM64x and the output is enabled when the boot mode is needed during a reset cycle and the input of buffer is connected to output of an I2C buffer set by the test automation circuit.

Table 2-16 List of Signals Routed to Test Automation Header J16
Signal Signal Type Function
POWER_DOWN GPIO Instructs the EVM to power down all circuits
PORZn GPIO Creates a PORz to the AM64X
WARM_RESETn GPIO Creates a RESETz to the AM64X
GPIO1 GPIO GPIO for communication with AM64X
GPIO2 GPIO GPIO for communication with AM64X
GPIO3 GPIO Used to Enable the BOOTMODE Buffer
GPIO4 GPIO Used to Reset the Boot mode IO Expander
Bootmode I2C0 I2C Communicates with boot mode I2C buffer
I2C1 I2C Communicates with AM64x

If the test automation circuit is going to control the boot mode, then all the switches have to be manually be set to the off position. The pins used for boot mode also have other functions, which is isolated by disabling the boot mode buffer during normal operation. Figure 2-12 shows the test automation signal connection with AM64x.

SK-AM64 SK-AM64B Test Automation Header Figure 2-12 Test Automation Header

Test Automation Header signals are optionally connected to the XDS110 microcontroller via zero ohm resistors. By default those resistors are made as DNI.

Table 2-17 Automation Header Signals Connected to XDS110
TM4C1294 Pin Name Signal Name
PM0 TEST_POWERDOWN
PM1 TEST_PORZn
PM2 TEST_WARMRESETn
PM3 TEST_GPIO1
PM4 TEST_GPIO2
PM5 TEST_GPIO3
PM6 TEST_GPIO4
PM7 TEST_POWERDOWN
PG0 TEST_PORZn
PG1 TEST_WARMRESETn

Table 2-18 lists test automation header’s pin-out and IO direction.

Table 2-18 Test Automation Header (J16) Pin-Outs
Pin No. Signal Name IO Direction (wrt SoC)
1 VCC3V3_TA Power (out)
2 VCC3V3_TA Power (out)
3 VCC3V3_TA Power (out)
4 NC NA
5 NC NA
6 NC NA
7 DGND Ground
8 NC NA
9 NC NA
10 NC NA
11 NC NA
12 NC NA
13 NC NA
14 NC NA
15 NC NA
16 DGND Ground
17 NC NA
18 NC NA
19 NC NA
20 NC NA
21 NC NA
22 NC NA
23 NC NA
24 NC NA
25 DGND Ground
26 TEST_POWERDOWN Input
27 TEST_PORZn Input
28 TEST_WARMRESETn Input
29 NC NA
30 TEST_GPIO1 Bidirectional
31 TEST_GPIO2 Bidirectional
32 TEST_GPIO3 Input
33 TEST_GPIO4 Input
34 DGND Ground
35 NC NA
36 SOC_I2C1_TA_SCL Bidirectional
37 BOOTMODE_I2C_SCL Bidirectional
38 SOC_I2C1_TA_SDA Bidirectional
39 BOOTMODE_I2C_SDA Bidirectional
40 DGND Ground
41 DGND Ground
42 DGND Ground