SPRUIY9C May 2021 – December 2025
There are 8 LED’s which are connected to an I2C Based LED Driver (TPIC2810D) which is controlled by the SoC via the I2C1 port. These 8 LED’s can be toggled based on the user application. Primarily these eight LEDs are meant for Industrial application.
Figure 2-22 Ethernet Interface - LEDs