SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
Table 6-28 lists the memory-mapped registers for the R5FSS_VIM module. All register offset addresses not listed in Table 6-28 should be considered as reserved locations and the register contents should not be modified.
| Instance | Base Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0000h(1) |
| R5FSS_VIC_CFG | 0FF8 0000h(2) |
| Offset | Acronym | Register Name | MCU_R5FSS_VIC_CFG Physical Address |
|---|---|---|---|
| 0h | Section 6.3.3.1 | Revision register | 40F8 0000h |
| 4h | Section 6.3.3.2 | Info register | 40F8 0004h |
| 8h | Section 6.3.3.3 | Prioritized IRQ register | 40F8 0008h |
| Ch | Section 6.3.3.4 | Prioritized FIQ register | 40F8 000Ch |
| 10h | Section 6.3.3.5 | IRQ group status register | 40F8 0010h |
| 14h | Section 6.3.3.6 | FIQ group status register | 40F8 0014h |
| 18h | Section 6.3.3.7 | IRQ vector address register | 40F8 0018h |
| 1Ch | Section 6.3.3.8 | FIQ vector address register | 40F8 001Ch |
| 20h | Section 6.3.3.9 | Active IRQ register | 40F8 0020h |
| 24h | Section 6.3.3.10 | Active FIQ register | 40F8 0024h |
| 30h | Section 6.3.3.11 | DED vector address register | 40F8 0030h |
| 400h + formula | Section 6.3.3.12 | Raw status/set register | 40F8 0400h + formula |
| 404h + formula | Section 6.3.3.13 | Interrupt enable status/clear register | 40F8 0404h + formula |
| 408h + formula | Section 6.3.3.14 | Interrupt enable set register | 40F8 0408h + formula |
| 40Ch + formula | Section 6.3.3.15 | Interrupt enabled clear register | 40F8 040Ch + formula |
| 410h + formula | Section 6.3.3.16 | IRQ interrupt enable status/clear register | 40F8 0410h + formula |
| 414h + formula | Section 6.3.3.17 | FIQ interrupt enable status/clear register | 40F8 0414h + formula |
| 418h + formula | Section 6.3.3.18 | Interrupt map register | 40F8 0418h + formula |
| 41Ch + formula | Section 6.3.3.19 | Interrupt type register | 40F8 041Ch + formula |
| 1000h + formula | Section 6.3.3.20 | Interrupt priority register | 40F8 1000h + formula |
| 2000h + formula | Section 6.3.3.21 | Interrupt vector register | 40F8 2000h + formula |
| Offset | Acronym | Register Name | R5FSS_VIC_CFG Physical Address |
|---|---|---|---|
| 0h | Section 6.3.3.1 | Revision register | 0FF8 0000h |
| 4h | Section 6.3.3.2 | Info register | 0FF8 0004h |
| 8h | Section 6.3.3.3 | Prioritized IRQ register | 0FF8 0008h |
| Ch | Section 6.3.3.4 | Prioritized FIQ register | 0FF8 000Ch |
| 10h | Section 6.3.3.5 | IRQ group status register | 0FF8 0010h |
| 14h | Section 6.3.3.6 | FIQ group status register | 0FF8 0014h |
| 18h | Section 6.3.3.7 | IRQ vector address register | 0FF8 0018h |
| 1Ch | Section 6.3.3.8 | FIQ vector address register | 0FF8 001Ch |
| 20h | Section 6.3.3.9 | Active IRQ register | 0FF8 0020h |
| 24h | Section 6.3.3.10 | Active FIQ register | 0FF8 0024h |
| 30h | Section 6.3.3.11 | DED vector address register | 0FF8 0030h |
| 400h + formula | Section 6.3.3.12 | Raw status/set register | 0FF8 0400h + formula |
| 404h + formula | Section 6.3.3.13 | Interrupt enable status/clear register | 0FF8 0404h + formula |
| 408h + formula | Section 6.3.3.14 | Interrupt enable set register | 0FF8 0408h + formula |
| 40Ch + formula | Section 6.3.3.15 | Interrupt enabled clear register | 0FF8 040Ch + formula |
| 410h + formula | Section 6.3.3.16 | IRQ interrupt enable status/clear register | 0FF8 0410h + formula |
| 414h + formula | Section 6.3.3.17 | FIQ interrupt enable status/clear register | 0FF8 0414h + formula |
| 418h + formula | Section 6.3.3.18 | Interrupt map register | 0FF8 0418h + formula |
| 41Ch + formula | Section 6.3.3.19 | Interrupt type register | 0FF8 041Ch + formula |
| 1000h + formula | Section 6.3.3.20 | Interrupt priority register | 0FF8 1000h + formula |
| 2000h + formula | Section 6.3.3.21 | Interrupt vector register | 0FF8 2000h + formula |
R5FSS_VIM_PID is shown in Figure 6-5 and described in Table 6-31.
Return to Summary Table.
This register contains the major and minor revisions for the module.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0000h |
| R5FSS_VIC_CFG | 0FF8 0000h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| REV | |||||||||||||||||||||||||||||||
| R-60900001h | |||||||||||||||||||||||||||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | REV | R | 60900001h | TI internal data. Identifies revision of peripheral. |
R5FSS_VIM_INFO is shown in Figure 6-6 and described in Table 6-33.
Return to Summary Table.
This contains information about the configuration of the R5FSS_VIM.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0004h |
| R5FSS_VIC_CFG | 0FF8 0004h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | INTERRUPTS | ||||||||||||||||||||||||||||||
| R-0h | R-200h | ||||||||||||||||||||||||||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 10-0 | INTERRUPTS | R | 200h | Indicates the number of interrupts supported by the VIM. |
R5FSS_VIM_PRIIRQ is shown in Figure 6-7 and described in Table 6-35.
Return to Summary Table.
This register contains the number of the highest priority pending IRQ.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0008h |
| R5FSS_VIC_CFG | 0FF8 0008h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| VALID | RESERVED | ||||||
| R-0h | R-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | PRI | ||||||
| R-0h | R-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | NUM | ||||||
| R-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| NUM | |||||||
| R-0h | |||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | VALID | R | 0h | This field indicates if the NUM field of this register is valid. |
| 30-20 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 19-16 | PRI | R | 0h | This field indicates the priority of the pending IRQ interrupt. |
| 15-10 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 9-0 | NUM | R | 0h | This field indicates the interrupt number of the pending IRQ interrupt with the highest priority. |
R5FSS_VIM_PRIFIQ is shown in Figure 6-8 and described in Table 6-37.
Return to Summary Table.
This register contains the number of the highest priority pending FIQ.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 000Ch |
| R5FSS_VIC_CFG | 0FF8 000Ch |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| VALID | RESERVED | ||||||
| R-0h | R-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | PRI | ||||||
| R-0h | R-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | NUM | ||||||
| R-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| NUM | |||||||
| R-0h | |||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | VALID | R | 0h | This field indicates if the NUM field of this register is valid. |
| 30-20 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 19-16 | PRI | R | 0h | This field indicates the priority of the pending FIQ interrupt. |
| 15-10 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 9-0 | NUM | R | 0h | This field indicates the interrupt number of the pending FIQ interrupt with the highest priority. |
R5FSS_VIM_IRQGSTS is shown in Figure 6-9 and described in Table 6-39.
Return to Summary Table.
This register indicates which groups of interrupts have pending, unmasked IRQ interrupts.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0010h |
| R5FSS_VIC_CFG | 0FF8 0010h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| STS | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | STS | R | 0h | This field indicates that one or more interrupts in group M are mapped to IRQ, unmasked, and pending. Bit 0 corresponds to group 0, bit 1 corresponds to group 1, etc. The interrupts associated with each group are [(M*32)+31:M*32] |
R5FSS_VIM_FIQGSTS is shown in Figure 6-10 and described in Table 6-41.
Return to Summary Table.
This register indicates which groups of interrupts have pending, unmasked FIQ interrupts.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0014h |
| R5FSS_VIC_CFG | 0FF8 0014h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| STS | |||||||||||||||||||||||||||||||
| R-0h | |||||||||||||||||||||||||||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | STS | R | 0h | This field indicates that one or more interrupts in group M are mapped to FIQ, unmasked, and pending. Bit 0 corresponds to group 0, bit 1 corresponds to group 1, etc. The interrupts associated with each group are [(M*32)+31:M*32] |
R5FSS_VIM_IRQVEC is shown in Figure 6-11 and described in Table 6-43.
Return to Summary Table.
This register contains the 32-bit interrupt vector address of the currently pending IRQ.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0018h |
| R5FSS_VIC_CFG | 0FF8 0018h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ADDR | RESERVED | ||||||||||||||||||||||||||||||
| R-0h | R-0h | ||||||||||||||||||||||||||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | ADDR | R | 0h | This field contains the upper 30 bits of the
32-bit interrupt vector address (addresses must be 32-bit
aligned) of the currently pending highest priority IRQ (as
indicated by the R5FSS_VIM_PRIIRQ[9-0] NUM field). |
| 1-0 | RESERVED | R | 0h | Reserved. Read as 0. The lower 2 bits of the 32-bit vector address are always 0. (Vector addresses must be 32-bit aligned.) |
R5FSS_VIM_FIQVEC is shown in Figure 6-12 and described in Table 6-45.
Return to Summary Table.
This register contains the 32-bit interrupt vector address of the currently pending FIQ.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 001Ch |
| R5FSS_VIC_CFG | 0FF8 001Ch |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ADDR | RESERVED | ||||||||||||||||||||||||||||||
| R-0h | R-0h | ||||||||||||||||||||||||||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | ADDR | R | 0h | This field contains the upper 30 bits of the
32-bit interrupt vector address (addresses must be 32-bit
aligned) of the currently pending highest priority FIQ (as
indicated by the R5FSS_VIM_PRIFIQ[9-0] NUM field). |
| 1-0 | RESERVED | R | 0h | Reserved. Read as 0. The lower 2 bits of the 32-bit vector address are always 0. (Vector addresses must be 32-bit aligned.) |
R5FSS_VIM_ACTIRQ is shown in Figure 6-13 and described in Table 6-47.
Return to Summary Table.
This register contains the number of the active IRQ.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0020h |
| R5FSS_VIC_CFG | 0FF8 0020h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| VALID | RESERVED | ||||||
| R-0h | R-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | PRI | ||||||
| R-0h | R-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | NUM | ||||||
| R-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| NUM | |||||||
| R-0h | |||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | VALID | R | 0h | This field indicates if the NUM field of this
register is valid. |
| 30-20 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 19-16 | PRI | R | 0h | This field indicates the priority of the active IRQ interrupt. |
| 15-10 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 9-0 | NUM | R | 0h | This field indicates the interrupt number of the
active IRQ interrupt. |
R5FSS_VIM_ACTFIQ is shown in Figure 6-14 and described in Table 6-49.
Return to Summary Table.
This register contains the number of the active FIQ.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0024h |
| R5FSS_VIC_CFG | 0FF8 0024h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| VALID | RESERVED | ||||||
| R-0h | R-0h | ||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | PRI | ||||||
| R-0h | R-0h | ||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | NUM | ||||||
| R-0h | R-0h | ||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| NUM | |||||||
| R-0h | |||||||
| LEGEND: R = Read Only; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | VALID | R | 0h | This field indicates if the NUM field of this
register is valid. |
| 30-20 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 19-16 | PRI | R | 0h | This field indicates the priority of the active FIQ interrupt. |
| 15-10 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 9-0 | NUM | R | 0h | This field indicates the interrupt number of the
active FIQ interrupt. |
R5FSS_VIM_DEDVEC is shown in Figure 6-15 and described in Table 6-51.
Return to Summary Table.
This register contains the 32-bit interrupt vector address to be used as a default in case of a DED error in any of the vectors.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0030h |
| R5FSS_VIC_CFG | 0FF8 0030h |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| ADDR | RESERVED | ||||||||||||||||||||||||||||||
| R/W-0h | R-0h | ||||||||||||||||||||||||||||||
| LEGEND: R = Read Only; R/W = Read/Write; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | ADDR | R/W | 0h | This field contains the upper 30 bits of the
32-bit interrupt vector address (the address must be 32-bit
aligned) of an interrupt to be used if an uncorrectable
double-bit error (DED) is detected in any of the interrupt
vector addresses. |
| 1-0 | RESERVED | R | 0h | Reserved. Read as 0. The lower 2 bits of the 32-bit vector address are always 0. (Vector addresses must be 32-bit aligned.) |
R5FSS_VIM_RAW_j is shown in Figure 6-16 and described in Table 6-53.
Return to Summary Table.
This register indicates the raw status of the events in group M.
Offset = 400h + (j * 20h); where j = 0h to Fh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0400h + formula |
| R5FSS_VIC_CFG | 0FF8 0400h + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| STS | |||||||||||||||||||||||||||||||
| R/W1S-0h | |||||||||||||||||||||||||||||||
| LEGEND: R/W1S = Read/Write 1 to Set Bit; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | STS | R/W1S | 0h | This is the raw status of the events in group M. Each bit corresponds to event Q, where Q = M*32+bit (example: bit 0 is event M*32+0, bit 1 is M*32+1, etc). |
R5FSS_VIM_STS_j is shown in Figure 6-17 and described in Table 6-55.
Return to Summary Table.
This register indicates the masked status of the events in group M.
Offset = 404h + (j * 20h); where j = 0h to Fh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0404h + formula |
| R5FSS_VIC_CFG | 0FF8 0404h + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MSK | |||||||||||||||||||||||||||||||
| R/W1C-0h | |||||||||||||||||||||||||||||||
| LEGEND: R/W1C = Read/Write 1 to Clear Bit; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | MSK | R/W1C | 0h | This is the masked status of the events in group M. Each bit corresponds to event Q, where Q = M*32+bit (example: bit 0 is event M*32+0, bit 1 is M*32+1, etc). |
R5FSS_VIM_INTR_EN_SET_j is shown in Figure 6-18 and described in Table 6-57.
Return to Summary Table.
This register is used to enable the mask for the events in group M.
Offset = 408h + (j * 20h); where j = 0h to Fh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0408h + formula |
| R5FSS_VIC_CFG | 0FF8 0408h + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MSK | |||||||||||||||||||||||||||||||
| R/W1S-0h | |||||||||||||||||||||||||||||||
| LEGEND: R/W1S = Read/Write 1 to Set Bit; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | MSK | R/W1S | 0h | This field is used to enable the mask of events in group M. Each bit corresponds to event Q, where Q = M*32+bit (example: bit 0 is event M*32+0, bit 1 is M*32+1, etc). |
R5FSS_VIM_INTR_EN_CLR_j is shown in Figure 6-19 and described in Table 6-59.
Return to Summary Table.
This register is used to disable the mask for the events in group M.
Offset = 40Ch + (j * 20h); where j = 0h to Fh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 040Ch + formula |
| R5FSS_VIC_CFG | 0FF8 040Ch + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MSK | |||||||||||||||||||||||||||||||
| R/W1C-0h | |||||||||||||||||||||||||||||||
| LEGEND: R/W1C = Read/Write 1 to Clear Bit; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | MSK | R/W1C | 0h | This field is used to disable the mask of events in group M. Each bit corresponds to event Q, where Q = M*32+bit (example: bit 0 is event M*32+0, bit 1 is M*32+1, etc). |
R5FSS_VIM_IRQSTS_j is shown in Figure 6-20 and described in Table 6-61.
Return to Summary Table.
This register indicates the masked status of the events in Group M that are also mapped as IRQs.
Offset = 410h + (j * 20h); where j = 0h to Fh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0410h + formula |
| R5FSS_VIC_CFG | 0FF8 0410h + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MSK | |||||||||||||||||||||||||||||||
| R/W1C-0h | |||||||||||||||||||||||||||||||
| LEGEND: R/W1C = Read/Write 1 to Clear Bit; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | MSK | R/W1C | 0h | This is the masked status of the events in group M that are mapped to IRQ. Each bit corresponds to event Q, where Q = M*32+bit (example: bit 0 is event M*32+0, bit 1 is M*32+1, etc). |
R5FSS_VIM_FIQSTS_j is shown in Figure 6-21 and described in Table 6-63.
Return to Summary Table.
This register indicates the masked status of the events in group M that are also mapped as FIQs.
Offset = 414h + (j * 20h); where j = 0h to Fh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0414h + formula |
| R5FSS_VIC_CFG | 0FF8 0414h + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MSK | |||||||||||||||||||||||||||||||
| R/W1C-0h | |||||||||||||||||||||||||||||||
| LEGEND: R/W1C = Read/Write 1 to Clear Bit; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | MSK | R/W1C | 0h | This is the masked status of the events in group M that are mapped to FIQ. Each bit corresponds to event Q, where Q = M*32+bit (example: bit 0 is event M*32+0, bit 1 is M*32+1, etc). |
R5FSS_VIM_INTMAP_j is shown in Figure 6-22 and described in Table 6-65.
Return to Summary Table.
This register is used to map interrupts as IRQ or FIQ.
Offset = 418h + (j * 20h); where j = 0h to Fh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 0418h + formula |
| R5FSS_VIC_CFG | 0FF8 0418h + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MSK | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| LEGEND: R/W = Read/Write; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | MSK | R/W | 0h | This field is used to indicate which interrupt the corresponding event influences (if enabled) for event group M. Each bit corresponds to event Q, where Q = M*32+bit (example: bit 0 is event M*32+0, bit 1 is M*32+1, etc). |
R5FSS_VIM_INTTYPE_j is shown in Figure 6-23 and described in Table 6-67.
Return to Summary Table.
This register indicates whether an interrupt is a pulse or level source.
Offset = 41Ch + (j * 20h); where j = 0h to Fh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 041Ch + formula |
| R5FSS_VIC_CFG | 0FF8 041Ch + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| MSK | |||||||||||||||||||||||||||||||
| R/W-0h | |||||||||||||||||||||||||||||||
| LEGEND: R/W = Read/Write; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-0 | MSK | R/W | 0h | This field is used to indicate whether the source of an interrupt is a level (default) or a pulse for event group M. Each bit corresponds to event Q, where Q = M*32+bit (example: bit 0 is event M*32+0, bit 1 is M*32+1, etc). |
R5FSS_VIM_PRI_INT_j is shown in Figure 6-24 and described in Table 6-69.
Return to Summary Table.
This register is used to set the priority of interrupt Q.
Offset = 1000h + (j * 4h); where j = 0h to 1FFh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 1000h + formula |
| R5FSS_VIC_CFG | 0FF8 1000h + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VAL | ||||||||||||||||||||||||||||||
| R-0h | R/W-Fh | ||||||||||||||||||||||||||||||
| LEGEND: R = Read Only; R/W = Read/Write; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved. Reads return 0. Writes have no effect. |
| 3-0 | VAL | R/W | Fh | This is the priority for interrupt Q. If two interrupts have the same priority, then whichever interrupt has the lower number Q wins arbitration. |
R5FSS_VIM_VEC_INT_j is shown in Figure 6-25 and described in Table 6-71.
Return to Summary Table.
This register contains the vector address associated with interrupt Q.
Offset = 2000h + (j * 4h); where j = 0h to 1FFh.
| Instance | Physical Address |
|---|---|
| MCU_R5FSS_VIC_CFG | 40F8 2000h + formula |
| R5FSS_VIC_CFG | 0FF8 2000h + formula |
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| VAL | RESERVED | ||||||||||||||||||||||||||||||
| R/W-0h | R-0h | ||||||||||||||||||||||||||||||
| LEGEND: R = Read Only; R/W = Read/Write; -n = value after reset |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | VAL | R/W | 0h | These are the upper 30 bits of the 32-bit vector
address associated with interrupt Q. It is the address that will
be reflected in the R5FSS_VIM_IRQVEC or R5FSS_VIM_FIQVEC and the
VECADDR output when interrupt Q is the active interrupt. |
| 1-0 | RESERVED | R | 0h | Reserved. Read as 0. The lower 2 bits of the 32-bit vector address are always 0. (Vector addresses must be 32-bit aligned.) |