SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The SRAM depth is separated in two segmets. The lower segment is reserved for indirect read use. The upper segment is for indirect write use only. The size of each segment is programmable via the OSPI_SRAM_PARTITION_CFG_REG register. This feature allows to allocate how many bits of the SRAM address bus are allocated to indirect read. By default, this is set so that exactly half of the SRAM is portioned for use by the indirect read controller. To ensure the read data bus is not directly fed by the SRAM read data through combinatorial logic, an extra bank of holding registers is included in the indirect read data path. These registers act as an extra location to be added to the allocated number of SRAM locations for indirect read.
To illustrate how the SRAM (and the extra bank of holding registers) can be allocated between indirect read and write, the following example is provided. The depth of the SRAM in this example is configured to be 8 bits. This is equal to 256 locations.
A value of 0xFF or 0x00 in the OSPI_SRAM_PARTITION_CFG_REG register should be avoided by software, as only the bottom 8 bits of the SRAM fill level are accessible through software (up to 255 limit) via the OSPI_SRAM_FILL_REG register. If the fill level reaches 256 on either the indirect read or write side, it will appear when reading the Fill Level to be 0.
There are four SRAM sources that are arbitrated and muxed onto the single SRAM port. Up to three sources can access this port at any one time. The sources are described as follows:
A fixed priority arbitration scheme is implemented. Table 12-215 shows priority allocated to these sources.
| SRAM Access Priority | |||
| Indirect Write | Write to SRAM (from System Data Bus) | 3rd (exclusive with Data Bus Read Request) | |
| Read from SRAM (from OSPI Module) | 2nd | ||
| Indirect Read | Write to SRAM (from OSPI Module) | 1st | |
| Read from SRAM (from System Data Bus) | 3rd (exclusive with Data Bus Write Request) | ||
With the exception of the write port during an Indirect Read operation (on the FLASH side of the SRAM), the logic driving all four sources must not assume single cycle completion. Writes to the SRAM during an indirect read must be allowed to complete immediately to avoid data loss. Therefore this port is given maximum priority.