SWRA601K April 2019 – November 2023 CC1350 , CC1352P , CC1352P7 , CC1352R , CC2340R5 , CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R , CC2642R-Q1 , CC2650 , CC2650MODA , CC2652P , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP
For regulatory approval testing it is typically required to configure the radio for static receiver and transmitter operation at certain frequencies. To facilitate such testing, the TI Bluetooth Low Energy/Bluetooth Low Energy 5 protocol stack implements the following HCI vendor-specific test commands:
For a full overview of the applicable HCI extension commands, parameters and associated events, see the HCI Vendor Specific Guide included with the Bluetooth Low Energy protocol stack documentation in the SDK.
The above commands can be invoked in a few different ways:
Additionally, the SmartRF Studio tool can be used to perform some of these tests. SmartRF™ Studio software does not rely upon any firmware on the device and instead directly controls the radio over a test interface (JTAG). However, for some regulatory testing purposes, the actual protocol stack firmware may be required.
Since regulatory testing requirements can vary from jurisdiction to jurisdiction, consult your test lab on specific test requirements based on where your product is sold.