DLPU075B october 2018 – april 2023 DLP2010 , DLPC3470 , DLPC3478
Table 3-48 describes the write parameters.
| Parameter Bytes | Description |
|---|---|
| Byte 1 | Pixels per line (LSByte) |
| Byte 2 | Pixels per line (MSByte) |
| Byte 3 | Lines per frame (LSByte) |
| Byte 4 | Lines per frame (MSByte) |
This command is used in conjunction with the Write Input Source Select command. This command specifies the active data size of the input image to the system for all external video interfaces, when the Write Input Source Select command selects external video port as the image source. The settings for this command are retained until changed using this command. These settings automatically apply each time the external video port is selected.
The parameter values are 1-based (for example, a value of 1280 pixels specifies 1280 pixels per line).
The user must review the notes for the Write Input Source Select command to understand the concept of source-associated commands. This concept determines when source-associated commands are executed by the system. This command is a source-associated command.
The maximum and minimum input values are shown in Table 3-49. The controller flags values outside of these ranges as an error (invalid command parameter), and does not execute the command.
| Parameter | Minimum Value | Maximum Value |
|---|---|---|
| Input source active pixels per line | 320 | 1280 |
| Input source active lines per frame | 200 | 800 |