DLPU075B october 2018 – april 2023 DLP2010 , DLPC3470 , DLPC3478
Table 3-21 describes the write parameters.
| Parameter Bytes | Description | Details |
|---|---|---|
| Byte 1 | Capture start pixel (LSByte) | Referenced to active data and 0-based (such that specifying the capture start pixel to be zero indicates the first active pixel of a line) |
| Byte 2 | Capture start pixel (MSByte) | |
| Byte 3 | Capture start line (LSByte) | Referenced to active data and 0-based (such that specifying the capture start line to be zero indicates the first active line of a frame) |
| Byte 4 | Capture start line (MSByte) | |
| Byte 5 | Pixels per line (LSByte) | 1-based (such that specifying a pixel per line value of 854 indicates 854 pixels to be captured) |
| Byte 6 | Pixels per line (MSByte) | |
| Byte 7 | Lines per frame (LSByte) | 1-based (such that specifying a lines per frame value of 480 indicates 480 lines to be captured) |
| Byte 8 | Lines per frame (MSByte) |
This command applies to all sources including test patterns, splash screens, and external sources. Making a change to the source or port does not impact the application of this command.
Cropping is done prior to the scaling function in the display module. As such, the size difference between the crop size and display size determines the amount of scaling needed in both dimensions. The scaling limits are listed in Table 3-22.
| Controller Configuration | Maximum Horizontal Interpolation Scale Factor | Maximum Horizontal Decimation Scale Factor | Maximum Vertical Interpolation Scale Factor | Maximum Vertical Decimation Scale Factor |
|---|---|---|---|---|
| Single controller (excluding interlaced NTSC/PAL) | 3.0 | 3.0 | 3.0 | 3.0 |
| Single controller (interlaced NTSC/PAL only) | 3.0 | 3.0 | 3.0 | 6.0 |
The scaling limits noted in Table 3-22 may not be possible depending on other factors, such as keystone correction. In this case, the system does what is requested even if this results in a broken image. The user is responsible for providing the appropriate input settings to meet the display needs.
If a crop size parameter exceeds the size of the input image, the input image size minus the capture start pixel/line is used (as shown in Figure 3-10). The crop size parameters returned by the read image crop command are always the values specified by the Write Image Crop command.
Figure 3-10 Cropping Rules when Crop Size exceeds Input Size