DLPU075B october 2018 – april 2023 DLP2010 , DLPC3470 , DLPC3478
Table 3-63 describes the return parameters.
| Parameter Bytes | Description |
|---|---|
| Byte 1 | Red LED current parameter (LSByte) |
| Byte 2 | Red LED current parameter (MSByte) |
| Byte 3 | Green LED current parameter (LSByte) |
| Byte 4 | Green LED current parameter (MSByte) |
| Byte 5 | Blue LED current parameter (LSByte) |
| Byte 6 | Blue LED current parameter (MSByte) |
The parameters returned by this command have a resolution of 10 bits, and are defined by the appropriate DLPA200x specification.
When the CAIC algorithm is enabled using the LED Output Control Method command:
Use of this command is only appropriate when the LED output control method is set to CAIC (automatic) RGB LED current control.
Unused most significant bits are set to 0.