DLPU113A December   2021  – April 2022 DLP2021-Q1

 

  1.   Trademarks
  2. 1DLP2021-Q1 Electronics EVM Overview
    1. 1.1 Introduction
    2. 1.2 What is in the DLP2021-Q1 Light Engine EVM
      1. 1.2.1 Formatter Subsystem
      2. 1.2.2 Illumination Subsystem
      3. 1.2.3 Light Engine
      4. 1.2.4 Cables
    3. 1.3 Non-Optical Specifications
      1. 1.3.1 Electrical Specifications
      2. 1.3.2 Component Temperature Ratings
      3. 1.3.3 LED Driver Design
      4. 1.3.4 Video Specification
  3. 2Quick Start
    1. 2.1 Kit Assembly Instructions
    2. 2.2 Software Installation
    3. 2.3 Power-Up
    4. 2.4 Select Display Content
    5. 2.5 LED Driver
  4. 3Optics and Mechanics
  5. 4Software
    1. 4.1 DLP Composer
      1. 4.1.1 Default Register Configuration
      2. 4.1.2 Illumination
      3. 4.1.3 Sequence Set
      4. 4.1.4 Degamma Curves
      5. 4.1.5 Image/Video
      6. 4.1.6 Flash Blocks
      7. 4.1.7 Flash Programming
    2. 4.2 DLP Control Program
      1. 4.2.1 Connection
      2. 4.2.2 Scripting
      3. 4.2.3 Registers
      4. 4.2.4 Commands
    3. 4.3 MSP430 Example Code
  6. 5Revision History

Flash Programming

After the DLP Composer project is configured as desired, use the Flash Programming page to program and verify the flash binary onto the SPI flash memory of the EVM.

GUID-ED6AD089-9EF8-4161-89BF-AF2D89D4C427-low.png Figure 4-7 DLP Composer - Flash Programming

Follow these steps to flash program the EVM:

  1. Start with the EVM powered-off.
  2. Set the SPI Adapter board to the Flash Programming operating mode.
  3. Connect the FTDI cable interface to the SPI Adapter Board and PC.
  4. Power-on the EVM. Figure 4-8 shows the LED status of the EVM when in the Flash Programming operation mode.
    GUID-20211206-SS0I-T8M1-ZRHS-J7P4WSXZTJHN-low.jpg Figure 4-8 Flash Programming Operating Mode LED Status
  5. Import and open the DLP2021LEQ1EVM DGP project in DLP Composer.
  6. Navigate to the Connections tab. Set to SPI and FTDI SPI Port, then click the Connect button. The virtual green LED should illuminate to indicate a successful connection as shown in Figure 4-9.
    GUID-509CF53E-FDED-4086-959C-F841FB9B8304-low.png Figure 4-9 DLP Composer - Connections
  7. Build the DLP Composer project using the Project → Build from the menu bar. Ensure the build is completed and successful before proceeding. Note, the build time will vary and can take up to several minutes depending on the size of the image/video content block.
  8. Navigate to the Flash Programming page, and browse to select the flash image file from the following directory: “(dgp_project_root)\Outputs\FlashImage.img”.
  9. Click the Program and Verify button to flash program the EVM. Note, the flash programming time will vary and can take up to several minutes depending on the size of the image/video content block.