DLPU113A December 2021 – April 2022 DLP2021-Q1
The formatter subsystem converts and translates image/video data stored in external flash memory through the FPGA based DMD controller into the Double Data Rate (DDR) interface format compatible with the DLP2021-Q1 data bus. The EVM offers two operating modes to specify what and how the image/video content is to be displayed: in a closed-loop stand-alone mode using the on-board MSP430 MCU, or through an external controller (such as the FTDI USB-to-SPI cable or Cheetahâ„¢ SPI Host Adapter) for GUI operation.
A DIP two-position switch at S1 on the DLP2021L1Q1EVM allows the user to physically set the operating mode of the formatter subsystem. The SPI Adapter board also has two physical switches (S1 and S2) to set the same operating modes. Figure 1-4 and Figure 1-5 show the default S1 switch state for Host Control operating mode for stand-alone operation, and the default switch state for Host Mute operating mode when the SPI Adapter Board is connected.
See Table 1-1 for the switch positions required of each operating mode.
Operating Mode | DLP2021LEQ1EVM | SPI Adapter Board | LED State | ||
---|---|---|---|---|---|
S1-A | S1-B | S1 | S2 | ||
Host Mute | OFF | ON | OFF | ON | Blue = ON, Amber = OFF, Green = ON |
Local Host Control | OFF | OFF | OFF | OFF | Blue = OFF, Amber = OFF, Green = ON |
FPGA Programming | ON | ON | ON | ON | Blue = ON, Amber = ON, Green = OFF |
Undefined | ON | OFF | ON | OFF | Blue = OFF, Amber = ON, Green = OFF |
A brief description of each operating mode is provided as follows:
To allow the SPI Adapter board to set the operating mode, TI recommends the DLP2021LEQ1EVM electronics board S1 switches always be set to Local Host Control mode. This is because the On-state of either board will always override the Off-state of the other board. This setup will enable the use the more easily accessible S1 and S2 toggle switches of the SPI Adapter board to set the operating modes. When the SPI Adapter board is detached, the EVM will automatically start-up in the Local Host Control mode to allow the MSP430 to configure and run the EVM without intervention from an external controller such as the FTDI cable. When switching between operating modes, TI recommends that the EVM be fully power cycled to reset and apply the most recently set operating mode.