SBAA661 February 2025 LMX1205
In the case of the signal being a sine wave, the relationship between slew rate (SR), frequency (f), and power (p) and these calculations are in Section 8 and the key relationship is as follows:
This equation implies that doubling the frequency doubles the slew rate and increasing the power by 6dB also doubles the slew rate and is shown in Figure 2-1.