SBAU230C August 2014 – March 2021 ADS8688
The PHI provides multiple power-supply options for the EVM, derived from the USB supply of the computer. The EEPROM on the ADS8688EVM uses a 3.3-V power supply generated directly by the PHI. The EVM_REG_5V5 is a 5.5V supply from the PHI and is applied to the input of a low dropout regulator (LDO) to generate AVDD on the EVM. The analog supply of the ADC (AVDD = 5.0V) is powered by the TPS7A4700RGWR (U3). The ADC Digital supply (DVDD = 3.3V), is generated by the PHI. Two LEDs are connected to the AVDD, and DVDD supplies. These LEDs will illuminate after the software GUI loads and the PHI turns on its output power supplies.
Figure 5-1 Power Supplies, Regulators, and Indicators