SBAU470 June 2026
Figure 4-3 shows the ADC Capture Settings page that allows easy configuration of multiple ADC settings and is an alternative method to using the Register Configurations page. The tab on the ADC Capture Settings page includes input channel selection, gain setting, system monitor selection, internal or external reference selection, filter selection, OSR configuration, IDAC selection and configuration. The ADC Capture Settings page has configuration to select internal reference voltage and speed mode, and the indicators for full scale range and data rate. Changing these settings updates the values on the Register Configurations page. Use the check box of Demo Mode in the upper right conner to disconnect or reconnect the ADS124S18EVM and the PAMB controller card to the GUI software. The green Connected indicator in the lower right corner in the GUI indicates the ADS124S18EVM and the PAMB controller card are successfully connected and communicating with the GUI software.
Figure 4-3 ADC Capture.