The following steps provides an overview to quickly get the ADS124S18EVM setup and operational. The subsequent sections in this document expand on each step to explain in detail the available features on the ADS124S18EVM and the corresponding GUI. Links below are provided to navigate from this quick-start guide to the appropriate section at each step, where applicable.
- Remove the ADS124S18EVM, PAMB controller card, and USB cable from the ADS124S18EVM-PDK box.
- If the PAMB controller card and the ADS124S18EVM are not already assembled, connect the ADS124S18EVM to the PAMB controller card as shown in the left image in Figure 1-2.
- Download the GUI from TI.com and install the GUI using the instructions in Section 3.2.
- Connect the micro-USB-to-USB cable from the PAMB directly to a USB port on the computer. Do not connect the USB cable through a USB hub.
- Open up the GUI software. Check if a green signal
displays and the hardware connected indicator shows in the bottom status ribbon
in the GUI (see Register
Configurations).
- Configure the internal registers from the Register
Configurations or ADC Capture Settings page in the GUI.
- Connect external sensors or signals to J4, J5, J7 or J8 on the ADS124S18EVM
as shown in Figure 1-1.
- Capture and analyze data by clicking the
Capture button on the Time Domain Display page in the GUI.