SBOA362A December   2019  – October 2026 REF34 , REF34-Q1 , REF3425-EP , REF3430-EP , REF3433-EP , REF3440-EP , REF4132-Q1 , REF50 , REF5020-EP , REF5020A-Q1 , REF5025-EP , REF5025-HT , REF5025A-Q1 , REF5030A-Q1 , REF5040-EP , REF5040A-Q1 , REF5045A-Q1 , REF5050-EP , REF5050A-Q1 , REF50E , REF70

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Voltage Reference Architecture
    1. 2.1 Shunt or Series Reference
    2. 2.2 Choosing the Best System Reference
  6. 3Key Specifications for Voltage Reference
    1. 3.1 Temperature Coefficient
    2. 3.2 Initial Accuracy
    3. 3.3 0.1–10 Hz Peak-to-peak Noise
    4. 3.4 Thermal Hysteresis and Long-term Stability
    5. 3.5 Load and Line Regulation
  7. 4Method of Negative Output Design and Noise Analysis
    1. 4.1 Voltage Inverting by Level Shift using REF5025 and OPA192
    2. 4.2 Using a Buffer to Generate Negative Reference Output
    3. 4.3 A Way to Minimize the Noise
  8. 5Conclusion
  9. 6References
  10. 7Revision History

Load and Line Regulation

Load regulation is the measure of the variation in VREF as a function of load current. It is specified either as a percentage, or in parts-per-million per milliamp (ppm/mA). It is calculated by dividing the relative change in VREF at the minimum and maximum load currents by the range of the load current. Load regulation depends on both the reference design and the parasitic resistance separating it from the load, so the reference must be placed as close to the load as the PCB layout allows.

The impedance of the reference input is large enough (> 10 kΩ) on many data converters that load regulation error may not be significant. Maximum load current information can be found in ADC or DAC data sheets as either a minimum reference pin resistance (RREF), or a maximum reference current (IREF). In situations where the reference is buffered with a high-speed op amp, load regulation error can usually be ignored. Line regulation applies only to series voltage references, and is the measure of the change in the reference voltage as a function of the input voltage. The importance of line regulation depends on the tolerance of the input supply, and may not contribute significantly to the total error in when the input voltage tolerance is within 10% or less.

As with line regulation, PSRR importance depends on input supply specifics. For example, the PSRR can be critical if the VIN is noisy due to a switching regulator, is sensitive to EMI, and is subject to large load transients.