SBOA602 November   2024 OPA593

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Current Booster, Push-Pull Topology Output Characteristics
    1. 2.1 Open-Loop Output Impedance
    2. 2.2 Minimizing Zero Crossover Distortion
  6. 3Various Current Booster Configurations
    1. 3.1 Complementary MOSFET versus BJT Current Booster Comparisons
  7. 4Stabilizing a Design for Power Amplifier Driving 1μF Capacitive Load (CL)
    1. 4.1 Op-Amp Driving Resistive Load
    2. 4.2 Op-Amp Driving Capacitive Load and Challenges
    3. 4.3 Open-Loop AC Stability Analysis - Compensating CL Effects Using DFC
    4. 4.4 Closed-Loop Stability Response - Small Signal Step Transient Analysis
    5. 4.5 Effects of Riso on Frequency Response in Dual Feedback Compensation
    6. 4.6 Summary of the DFC Technique
  8. 5Stabilizing the OPA593 and Darlington Current Booster for 1μF Capacitive Load
    1. 5.1 Open-Loop AC Stability Analysis - Composite Op-Amp Driving 1μF CL
    2. 5.2 Closed-Loop Stability Response - Composite Op-Amp's Step Transient Analysis
  9. 6Composite Amplifier's Effective BW and Step Time Response
  10. 7Test Bench Validation
  11. 8Summary
  12. 9References

Minimizing Zero Crossover Distortion

A simplified current booster without a preconfigured forward bias can be adequate for voltage regulators with discrete setpoints; however, a simplified current booster is not designed for applications that require minimal non-linearity and distortion. In a Darlington configuration, a dead zone of approximately 1.3V occurs when the transistors do not receive sufficient biased voltage, resulting in a lack of output current amplification and exhibiting a cutoff characteristic. This situation can delay the step response, as the booster must first overcome the VBE threshold. Adding a zero-crossover resistor, RZRO (for example, 1-10kΩ), can alleviate this dead zone, as shown in Figure 2-3, allowing some output current to flow even when the transistors are non-conductive. This modification does not affect the open-loop output impedance, as shown in Figure 2-4.

 Minimize Crossover Distortion with Zero-Crossover Resistor (RZCO)Figure 2-3 Minimize Crossover Distortion with Zero-Crossover Resistor (RZCO)

By placing a 10kΩ zero-crossover resistor (RZRO) inside the common emitter current booster, as shown in Figure 2-4, the open-loop output impedance of the current booster driver remains unaffected.

 Open-Loop Output Impedance Remains Unaffected by RZCOFigure 2-4 Open-Loop Output Impedance Remains Unaffected by RZCO