SBOA602 November   2024 OPA593

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Current Booster, Push-Pull Topology Output Characteristics
    1. 2.1 Open-Loop Output Impedance
    2. 2.2 Minimizing Zero Crossover Distortion
  6. 3Various Current Booster Configurations
    1. 3.1 Complementary MOSFET versus BJT Current Booster Comparisons
  7. 4Stabilizing a Design for Power Amplifier Driving 1μF Capacitive Load (CL)
    1. 4.1 Op-Amp Driving Resistive Load
    2. 4.2 Op-Amp Driving Capacitive Load and Challenges
    3. 4.3 Open-Loop AC Stability Analysis - Compensating CL Effects Using DFC
    4. 4.4 Closed-Loop Stability Response - Small Signal Step Transient Analysis
    5. 4.5 Effects of Riso on Frequency Response in Dual Feedback Compensation
    6. 4.6 Summary of the DFC Technique
  8. 5Stabilizing the OPA593 and Darlington Current Booster for 1μF Capacitive Load
    1. 5.1 Open-Loop AC Stability Analysis - Composite Op-Amp Driving 1μF CL
    2. 5.2 Closed-Loop Stability Response - Composite Op-Amp's Step Transient Analysis
  9. 6Composite Amplifier's Effective BW and Step Time Response
  10. 7Test Bench Validation
  11. 8Summary
  12. 9References

Closed-Loop Stability Response - Composite Op-Amp's Step Transient Analysis

To assess the closed-loop behavior of the compensated OPA593 in the current booster configuration, a small signal step transient analysis was performed, as shown in Figure 5-5. The closed-loop transient response reveals no overshoot or oscillation, indicating a sufficient phase margin and effective compensation applied to the inner and outer feedback loops.

 Compensated Composite Amplifier - Step Transient Response in Time DomainFigure 5-5 Compensated Composite Amplifier - Step Transient Response in Time Domain

Like the emulated power amplifier in Section 4, gain peaking or Q effects can be more pronounced in actual op-amp simulations. Each op-amp design contains numerous hidden poles and zeros. While these high frequency poles and zeros typically do not interfere with single feedback loop compensation within the UGBW, the DFC compensation methods can be an exception, particularly when managing multiple feedback loops. Thus, it is crucial to examine the AC frequency response behavior, to verify sweep frequency response in ATE applications, as shown in Figure 5-6.

 OPA593 and Current Booster's Effective Bandwidth: AC Sweep in Frequency DomainFigure 5-6 OPA593 and Current Booster's Effective Bandwidth: AC Sweep in Frequency Domain