SBOA602 November   2024 OPA593

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Current Booster, Push-Pull Topology Output Characteristics
    1. 2.1 Open-Loop Output Impedance
    2. 2.2 Minimizing Zero Crossover Distortion
  6. 3Various Current Booster Configurations
    1. 3.1 Complementary MOSFET versus BJT Current Booster Comparisons
  7. 4Stabilizing a Design for Power Amplifier Driving 1μF Capacitive Load (CL)
    1. 4.1 Op-Amp Driving Resistive Load
    2. 4.2 Op-Amp Driving Capacitive Load and Challenges
    3. 4.3 Open-Loop AC Stability Analysis - Compensating CL Effects Using DFC
    4. 4.4 Closed-Loop Stability Response - Small Signal Step Transient Analysis
    5. 4.5 Effects of Riso on Frequency Response in Dual Feedback Compensation
    6. 4.6 Summary of the DFC Technique
  8. 5Stabilizing the OPA593 and Darlington Current Booster for 1μF Capacitive Load
    1. 5.1 Open-Loop AC Stability Analysis - Composite Op-Amp Driving 1μF CL
    2. 5.2 Closed-Loop Stability Response - Composite Op-Amp's Step Transient Analysis
  9. 6Composite Amplifier's Effective BW and Step Time Response
  10. 7Test Bench Validation
  11. 8Summary
  12. 9References

Stabilizing the OPA593 and Darlington Current Booster for 1μF Capacitive Load

The design approach using the OPA593 with a Darlington current booster topology for driving 1µF capacitive load follows the dual feedback compensation (DFC) process designed for the emulated power amplifier, shown in Figure 4-5. A key difference is that the current booster effectively acts as the isolation resistor (Riso) in the designed emulated PA example. While the OPA593 maintains an output impedance of approximately 228Ω from 1kHz to 1MHz, this is not designed for driving large capacitive loads using the compensation technique outlined in Table 4-4, where alternative DFC compensation techniques are more appropriate.

The design requirements for the OPA593 and the current booster configuration are detailed in Table 2-2 at the beginning of the article. Integrating the OPA593 with a Darlington current booster creates a composite amplifier with low open-loop output impedance. This composite amplifier benefits from the OPA593’s performance attributes—such as high input voltage handling, high slew rate, current limiting, and Enable or Disable functionality. These features make the OPA593 capable of driving large capacitive loads and meeting high current demands in ATE applications, provided that the feedback network is properly compensated.

In the current booster configuration shown in Figure 5-1, simulations reveal that the unity gain bandwidth, funity of the OPA593 combined with the Darlington current booster remains consistent, with a measured funity of approximately 1.4MHz and a phase margin of 79°. When the gain bandwidth product is applied, the simulation results closely match those of the emulated power amplifier depicted in Figure 4-1. This suggests that the closed-loop of the composite amplifier needs to exhibit similar behaviors as the emulated power amplifier.

 OPA593 + Current Booster Driving Resistive Load with VREF = 1VdcFigure 5-1 OPA593 + Current Booster Driving Resistive Load with VREF = 1Vdc