SBOU211A October 2018 – July 2025
There are multiple methods of applying a reference voltage to the device. The reference voltage is set by J9, which either connects the reference to ground or ties the reference to the output of the reference buffer. The reference buffer is initially configured to generate a rail at mid-supply for single supply operation. Alternatively, this jumper can be left unconnected and the desired voltage can be applied directly to the VREF test point. It is also possible to connect J7 and configure the reference buffer as an integrator to ac couple the output as shown in Figure 2-3.