SBOU319A November 2024 – June 2025 HDC3120
The heater enable switch is a sliding style mechanism which when moved to the 'ON' position, a red LED (D1) illuminates to indicate the heater is running and the user must observe the temperature output increasing while humidity decreases. After the heater has been switched off, press the reset button (SW1) before reading temperature and humidity outputs to verify consistent readings.
During heater operation, avoid contact with the HDC3120 as the temperature can exceed 55°C. Additionally, running the heater for an extended period of time is not recommended to avoid potential damage to the sensor.