SCDA058 September   2025 TMUX1575 , TMUX4827 , TMUX7612 , TS5A22362 , TS5A22364

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2What is THD
  6. 3What is THD + N
  7. 4THD(+N) of Multiplexers
    1. 4.1 Understanding THD(+N) of a Multiplexer
  8. 5Low THD Multiplexer Applications
  9. 6Low THD Mux Device Recommendations
  10. 7Summary
  11. 8References

Understanding THD(+N) of a Multiplexer

For multiplexed systems, the observed THD(+N) performance is a function of the On-Resistance (RON), RON flatness (variation of the mux channel RON across the applied signal range) of the device and the load resistance, RL. As the ratio RL/RON increases the THD+N performance improves. This is due to the creation of an amplitude-dependent voltage divider, as shown in Figure 4-2, through the combination of Ron and RL. This follows then that the observed harmonic distortion of the mux output is minimized when RL is larger, such as a high impedance input of a non-inverting amplifier.

 Voltage Divider Created by MUX RON and RLFigure 4-2 Voltage Divider Created by MUX RON and RL

Typically, for applications where THD matters, the operational peak-to-peak voltage range can be a smaller range than the full voltage swing the mux is capable of. Therefore, this is important to verify that the operating voltage of a device does not fall in a region where the RON of the mux varies greatly. Some Ron curves are flat across the entire region, while others can have optimized performance across a specific input voltage region. Figure 4-3 shows how the same device can have different THD performance, given different operational peak-to-peak (Vpp) voltages.

 RON Curve With Optimized (Green) Vpp Region vs Unoptimized (Red) Vpp RegionFigure 4-3 RON Curve With Optimized (Green) Vpp Region vs Unoptimized (Red) Vpp Region

To optimize THD performance, the recommendation is to use the RON region of the multiplexer that is the flattest. Figure 4-4, shows the optimized THD Regions for common of RON curves for analog multiplexers. Figure 4-5 highlights how an ultra-flat RON optimizes THD performance in the TMUX4827.

 Best Region (Green) of VIN for Optimized THD Performance Figure 4-4 Best Region (Green) of VIN for Optimized THD Performance
 TMUX4827 Achieves Optimized THD Performance Through Ultra-Flat RONFigure 4-5 TMUX4827 Achieves Optimized THD Performance Through Ultra-Flat RON